Skip to main content
brubinstein
Associate II
March 10, 2015
Question

DMA works only first time

  • March 10, 2015
  • 3 replies
  • 916 views
Posted on March 10, 2015 at 22:16

Hi,

I'm using ADC and DMA. For learning purposes no interrupts, just polling LIFR. Staring conversion with ADC_CR2_SWSTART. As soon as TCIF is set,  I'm writing 1 to ALL flags to LIFCR (LIFR becomes 0) then re-enabling DMA. Do ADC_CR2_SWSTART again and no more flags in LIFR...EOC flag for ADC is set.

Why is that? What am I missing?

#dma
This topic has been closed for replies.

3 replies

waclawek.jan
Super User
March 10, 2015
Posted on March 10, 2015 at 23:52

I don't know ( I never used DMA with ADC), but maybe you might want to try to play with something like a simple timer (*not* the advanced like TIM1/TIM8) or USART. ADC might have its own issues, and/or the bits enabling DMA in the ADC.

Also, look at the DMA registers after the ''restart'', post them here if you want.

JW

brubinstein
Associate II
March 11, 2015
Posted on March 11, 2015 at 01:43

All DMA registers are the same as they were before the first time i.e after init().

DMA after    init()         first successful  Before the next

                            transfer          transfer

LISR         0              0x00000C00        0 

HISR         0              0                 0  

S1CR         0x04002C01     0x04002C00        0x04002C01

S1NDTR       0x4            0                 0x04

S1PAR        0x4001224C     0x4001224C        0x4001224C

S1M0AR       0x20000000     0x20000000        0x20000000

S1FCR        0x00000020     0x00000020        0x00000020

ADC3                                          DMA is looping  

SR           0              0x00000010        0x00000012

CR1          0x03000100     0x03000100        0x03000100 

CR2          0x00000101     0x00000101        0x00000101

waclawek.jan
Super User
March 11, 2015
Posted on March 11, 2015 at 09:11

Nice catch, Baruch!

Indeed, the text in ADC chapter contains this:

 

No new DMA request is issued to the DMA controller if the DDS bit is cleared to 0 in the

 

ADC_CR2 register (this avoids generating an overrun error). However the DMA bit is

 

not cleared by hardware. It must be written to 0, then to 1 to start a new transfer.

 

A hidden bit influencing hardware's behaviour is an, ehm, really bad idea, if you ask me...

Thanks for sharing this info.

JW