Question
DMA with read strobe but without write strobe
Posted on May 19, 2014 at 03:47
Hi All
STM32F2xx:I assume this is not possible but....Can a DMA transaction have the read strobe only without the write strobe (ie half the transaction)?The reason is due to our project having an FPGA being mapped onto a SRAM bank.Therefore to DMA from external memory into the FPGA, we need to read into the STM then write out again to the FPGA.If we can use just the read-half of a STM DMA transaction, the STM nOE can be used as the nWR strobe into the FPGA - this then doubles bandwidth.(The other option is to have the FPGA also as a DMA master loading directly from SRAM, but that introduces timing/contention complexities and defeats the purpose of already having a DMA master in the STM)ThxJas