DMA using USART3 on STM32H7 part
I am trying to get the USART3 to work with DMA, and so far have been unable to. After the initial cubeIDE project setup, I verified that standard (non DMA) RX and TX were working fine.
Moving to DMA, I was getting Direct Mode Error interrupts, and a little bit of digging showed me that the buffers I was using to send data were located in the DTCM ram. Changing that to move it to the D2 Space (starting at 0x3000000), and verifying the map file, I don't get Direct mode error interrupts, but I get no transmission of any bytes either.
Any thoughts or suggestions as to why DMA would not work on usart3? (FYI, I am using DMA successfuly on the SAI peripheral, so I know that DMA2 is working - USART uses DMA1). Thanks