Skip to main content
ilyaz yilmaz
Associate II
April 27, 2020
Question

DMA USART callback function

Hello,

Stm32 F401RE Hal Library 2016 Works.

Stm32 F401RE Hal Library 2017(last version) DOESNT Works.

For Test purpose only I use USART DMA Send function. Main.C is like that...

Also This StMicroelectrincs youtube vide work 2016 HAL Library but it doesnt work 2017 Hal Library. Video is very simple actually. I test it maybe 10 times. but 2017 Hal Library doesnt work.

https://www.youtube.com/watch?v=BxFYmBYBmaU

/* Private user code ---------------------------------------------------------*/

/* USER CODE BEGIN 0 */

uint8_t data_tx[5] = {0x41 , 0x42 ,0x43 ,0x44 , 0x45};

/* USER CODE END 0 */

/**

 * @brief The application entry point.

 * @retval int

 */

int main(void)

{

 /* USER CODE BEGIN 1 */

 /* USER CODE END 1 */

 /* MCU Configuration--------------------------------------------------------*/

 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */

 HAL_Init();

 /* USER CODE BEGIN Init */

 /* USER CODE END Init */

 /* Configure the system clock */

 SystemClock_Config();

 /* USER CODE BEGIN SysInit */

 /* USER CODE END SysInit */

 /* Initialize all configured peripherals */

 MX_GPIO_Init();

 MX_DMA_Init();

 MX_USART2_UART_Init();

 MX_USART1_UART_Init();

 /* USER CODE BEGIN 2 */

 /* USER CODE END 2 */

 /* Infinite loop */

 /* USER CODE BEGIN WHILE */

 while (1)

 {

   /* USER CODE END WHILE */

   /* USER CODE BEGIN 3 */

    HAL_GPIO_TogglePin(LD2_GPIO_Port, LD2_Pin);

    HAL_UART_Transmit_DMA(&huart1, data_tx, 5);

    HAL_Delay(500);

 }

 /* USER CODE END 3 */

}

/* USER CODE BEGIN 4 */

uint64_t cnt1;

void HAL_UART_TxCpltCallback(UART_HandleTypeDef *huart)

{

   cnt1++;

}

/* USER CODE END 4 */

I Will also add interrupt file

extern DMA_HandleTypeDef hdma_usart1_rx;

extern DMA_HandleTypeDef hdma_usart1_tx;

/* USER CODE BEGIN EV */

/* USER CODE END EV */

/******************************************************************************/

/*          Cortex-M4 Processor Interruption and Exception Handlers         */

/******************************************************************************/

/**

 * @brief This function handles Non maskable interrupt.

 */

void NMI_Handler(void)

{

 /* USER CODE BEGIN NonMaskableInt_IRQn 0 */

 /* USER CODE END NonMaskableInt_IRQn 0 */

 /* USER CODE BEGIN NonMaskableInt_IRQn 1 */

 /* USER CODE END NonMaskableInt_IRQn 1 */

}

/**

 * @brief This function handles Hard fault interrupt.

 */

void HardFault_Handler(void)

{

 /* USER CODE BEGIN HardFault_IRQn 0 */

 /* USER CODE END HardFault_IRQn 0 */

 while (1)

 {

   /* USER CODE BEGIN W1_HardFault_IRQn 0 */

   /* USER CODE END W1_HardFault_IRQn 0 */

 }

}

/**

 * @brief This function handles Memory management fault.

 */

void MemManage_Handler(void)

{

 /* USER CODE BEGIN MemoryManagement_IRQn 0 */

 /* USER CODE END MemoryManagement_IRQn 0 */

 while (1)

 {

   /* USER CODE BEGIN W1_MemoryManagement_IRQn 0 */

   /* USER CODE END W1_MemoryManagement_IRQn 0 */

 }

}

/**

 * @brief This function handles Pre-fetch fault, memory access fault.

 */

void BusFault_Handler(void)

{

 /* USER CODE BEGIN BusFault_IRQn 0 */

 /* USER CODE END BusFault_IRQn 0 */

 while (1)

 {

   /* USER CODE BEGIN W1_BusFault_IRQn 0 */

   /* USER CODE END W1_BusFault_IRQn 0 */

 }

}

/**

 * @brief This function handles Undefined instruction or illegal state.

 */

void UsageFault_Handler(void)

{

 /* USER CODE BEGIN UsageFault_IRQn 0 */

 /* USER CODE END UsageFault_IRQn 0 */

 while (1)

 {

   /* USER CODE BEGIN W1_UsageFault_IRQn 0 */

   /* USER CODE END W1_UsageFault_IRQn 0 */

 }

}

/**

 * @brief This function handles System service call via SWI instruction.

 */

void SVC_Handler(void)

{

 /* USER CODE BEGIN SVCall_IRQn 0 */

 /* USER CODE END SVCall_IRQn 0 */

 /* USER CODE BEGIN SVCall_IRQn 1 */

 /* USER CODE END SVCall_IRQn 1 */

}

/**

 * @brief This function handles Debug monitor.

 */

void DebugMon_Handler(void)

{

 /* USER CODE BEGIN DebugMonitor_IRQn 0 */

 /* USER CODE END DebugMonitor_IRQn 0 */

 /* USER CODE BEGIN DebugMonitor_IRQn 1 */

 /* USER CODE END DebugMonitor_IRQn 1 */

}

/**

 * @brief This function handles Pendable request for system service.

 */

void PendSV_Handler(void)

{

 /* USER CODE BEGIN PendSV_IRQn 0 */

 /* USER CODE END PendSV_IRQn 0 */

 /* USER CODE BEGIN PendSV_IRQn 1 */

 /* USER CODE END PendSV_IRQn 1 */

}

/**

 * @brief This function handles System tick timer.

 */

void SysTick_Handler(void)

{

 /* USER CODE BEGIN SysTick_IRQn 0 */

 /* USER CODE END SysTick_IRQn 0 */

 HAL_IncTick();

 /* USER CODE BEGIN SysTick_IRQn 1 */

 /* USER CODE END SysTick_IRQn 1 */

}

/******************************************************************************/

/* STM32F4xx Peripheral Interrupt Handlers                                   */

/* Add here the Interrupt Handlers for the used peripherals.                 */

/* For the available peripheral interrupt handler names,                     */

/* please refer to the startup file (startup_stm32f4xx.s).                   */

/******************************************************************************/

/**

 * @brief This function handles DMA2 stream2 global interrupt.

 */

void DMA2_Stream2_IRQHandler(void)

{

 /* USER CODE BEGIN DMA2_Stream2_IRQn 0 */

 /* USER CODE END DMA2_Stream2_IRQn 0 */

 HAL_DMA_IRQHandler(&hdma_usart1_rx);

 /* USER CODE BEGIN DMA2_Stream2_IRQn 1 */

 /* USER CODE END DMA2_Stream2_IRQn 1 */

}

/**

 * @brief This function handles DMA2 stream7 global interrupt.

 */

void DMA2_Stream7_IRQHandler(void)

{

 /* USER CODE BEGIN DMA2_Stream7_IRQn 0 */

 /* USER CODE END DMA2_Stream7_IRQn 0 */

 HAL_DMA_IRQHandler(&hdma_usart1_tx);

 /* USER CODE BEGIN DMA2_Stream7_IRQn 1 */

 /* USER CODE END DMA2_Stream7_IRQn 1 */

}

/* USER CODE BEGIN 1 */

/* USER CODE END 1 */

/************************ (C) COPYRIGHT STMicroelectronics *****END OF FILE****/

This topic has been closed for replies.

11 replies

waclawek.jan
Super User
April 27, 2020

What exactly"doesn't work" means?

Read out and check/compare between working/not working the relevant USART/DMA/GPIO registers.

JW

ilyaz yilmaz
Associate II
April 27, 2020

Ohhh I forgot to write ,

Dma function send data but Callback completed function doesnt work. below function..

/* USER CODE BEGIN 4 */

uint64_t cnt1;

void HAL_UART_TxCpltCallback(UART_HandleTypeDef *huart)

{

   cnt1++;

}

/* USER CODE END 4 */

And it transmit only one time second time it doesnt transmit. Because dma stay busy state.

But same code works with 2016 Hal Library.

FNass.1
Visitor II
November 27, 2020

Hi,

Dma counter must be re-initailized in order to transmit again.

Best regards...

FEN

TDK
April 27, 2020

I would use the latest HAL library instead of 3-4 year old versions.

"If you feel a post has answered your question, please click ""Accept as Solution""."
ilyaz yilmaz
Associate II
April 27, 2020

2017 is the latest hal library...

it correspond to firmvare STM32Cube_FW_F4_V1.25.0

and it s the last firmware.

TDK
April 27, 2020

> 2017 is the latest hal library...

> it correspond to firmvare STM32Cube_FW_F4_V1.25.0

> and it s the last firmware.

I agree that v1.25.0 is the latest firmware, but why are you referring to it as "Hal Library 2017"? It was released February 12, 2020.

"If you feel a post has answered your question, please click ""Accept as Solution""."
ilyaz yilmaz
Associate II
April 27, 2020

Ok.I will explain why I said 2017 dma hal library.

In the source code which doesnt work (stm32f4xx_hal_dma.c) There is comment like that....

******************************************************************************
 
 * @attention
 
 *
 
 * <h2><center>&copy; Copyright (c) 2017 STMicroelectronics.
 
 * All rights reserved.</center></h2>
 
 *
 
 * This software component is licensed by ST under BSD 3-Clause license,
 
 * the "License"; You may not use this file except in compliance with the
 
 * License. You may obtain a copy of the License at:
 
 * opensource.org/licenses/BSD-3-Clause
 
 *
 
 ******************************************************************************
 
 */ 

In the source code which works (stm32f4xx_hal_dma.c) There is comment like that....

 ******************************************************************************
 * @attention
 *
 * <h2><center>&copy; COPYRIGHT(c) 2016 STMicroelectronics</center></h2>
 *
 * Redistribution and use in source and binary forms, with or without modification,
 * are permitted provided that the following conditions are met:
 * 1. Redistributions of source code must retain the above copyright notice,
 * this list of conditions and the following disclaimer.
 * 2. Redistributions in binary form must reproduce the above copyright notice,
 * this list of conditions and the following disclaimer in the documentation
 * and/or other materials provided with the distribution.
 * 3. Neither the name of STMicroelectronics nor the names of its contributors
 * may be used to endorse or promote products derived from this software
 * without specific prior written permission.
 *
 * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
 * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE
 * IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE
 * DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT HOLDER OR CONTRIBUTORS BE LIABLE
 * FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL
 * DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR
 * SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER
 * CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY,
 * OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
 * OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
 *
 ******************************************************************************
 */ 

So I write the 2017 and 2016 years. But Firmware 1.25.0 doesnt work as expected in dma.Transmit and receive.

But older firmware I dont know exactly whic version it's working.

Piranha
Principal III
April 28, 2020

Could be related to USE_HAL_UART_REGISTER_CALLBACKS.

Anyway it's HAL - overcomplex non-working bloatware with unusable architecture. Toss it out and invest your time in learning real development:

https://github.com/MaJerle/stm32-usart-uart-dma-rx-tx

ilyaz yilmaz
Associate II
April 28, 2020

I agree with you about Hal Libraries. They could be more reliabable and bare...

Anyway I realize that.Hal Library only call callback function in circular mode.

static void UART_DMATransmitCplt(DMA_HandleTypeDef *hdma)
{
 UART_HandleTypeDef *huart = (UART_HandleTypeDef *)((DMA_HandleTypeDef *)hdma)->Parent;
 /* DMA Normal mode*/
 if ((hdma->Instance->CR & DMA_SxCR_CIRC) == 0U)
 {
 
 huart->TxXferCount = 0x00U;
 
 /* Disable the DMA transfer for transmit request by setting the DMAT bit
 in the UART CR3 register */
 CLEAR_BIT(huart->Instance->CR3, USART_CR3_DMAT);
 
 /* Enable the UART Transmit Complete Interrupt */
 SET_BIT(huart->Instance->CR1, USART_CR1_TCIE);
	#if (USE_HAL_UART_REGISTER_CALLBACKS == 1)
		/*Call registered Tx complete callback*/
		huart->TxCpltCallback(huart);
	#else
		/*Call legacy weak Tx complete callback*/
		HAL_UART_TxCpltCallback(huart);
	#endif /* USE_HAL_UART_REGISTER_CALLBACKS */
 
 
 }
 /* DMA Circular mode */
 else
 {
#if (USE_HAL_UART_REGISTER_CALLBACKS == 1)
 /*Call registered Tx complete callback*/
 huart->TxCpltCallback(huart);
#else
 /*Call legacy weak Tx complete callback*/
 HAL_UART_TxCpltCallback(huart);
#endif /* USE_HAL_UART_REGISTER_CALLBACKS */
 }
}

ilyaz yilmaz
Associate II
April 28, 2020

https://github.com/MaJerle/stm32-usart-uart-dma-rx-tx

Also this sample uses Low layer api.

You advie to use LL insetead of HAL.

ilyaz yilmaz
Associate II
April 28, 2020

In firmware version 1.25 usart tx DMA in normal mode doesnt call usart_tx_completed callback function.(But in old firmware it was called)

I dont know the solution is true or not. But when enable usart global interrupt it call the function.

Old and new HAL library works different. Maybe it's bug or new way I dont know.

We will understand if ST make example with new firmware DMA and usart.

Thanks for reply Everyone...