Skip to main content
Reed Thompson
Associate
January 2, 2018
Question

DMA update request to ADC works with timer 2 but not with timer 6 on stm32f7

  • January 2, 2018
  • 2 replies
  • 649 views
Posted on January 02, 2018 at 03:06

DMA update request to ADC works with timer 2 but not with timer 6 on stm32f7. The data sheet states that timer 6 should be able to generate a DMA request in section 25.2 in document RM0385. Can anyone confirm this is possible? I don't mind using timer 2 but for curiosity's sake. 

    This topic has been closed for replies.

    2 replies

    Tesla DeLorean
    Guru
    January 2, 2018
    Posted on January 02, 2018 at 03:37

    Section 25.2 in RM0385 Rev 6 talks about the DAC not the ADC

    http://www.st.com/content/ccc/resource/technical/document/reference_manual/c5/cf/ef/52/c0/f1/4b/fa/DM00124865.pdf/files/DM00124865.pdf/jcr:content/translations/en.DM00124865.pdf

     

    You want the ADC to trigger the DMA, and the TIM to trigger the ADC

    Table 94 (section 15.6) described the ADC's External Trigger. TIM6_TRGO is mentioned, so you'd need to configure TIM6 and route one of the sources (Update, CC1, CC2, etc) to the TRGO (Trigger Output) functionality.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Reed Thompson
    Associate
    January 2, 2018
    Posted on January 02, 2018 at 04:03

    Right, that was the idea. I am usingTIM6 to count up and then cause an update event. This then causes the ADC to convert and then send a DMA request to send the data to my buffer. I set an interruptHAL_ADC_ConvCpltCallback( ) andHAL_TIM_PeriodElapsedCallback( ) with nop's in them just to hit the breakpoint and prove I got somewhere or not. I always get to

    HAL_TIM_PeriodElapsedCallback( ) but never break on HAL_ADC_ConvCpltCallback( ). When I use TIM2 or TIM8 it does work.

    so as an implementation:

    I use this in main( )

    HAL_ADC_Start_DMA(&hadc1, (uint32_t*)rawData, bufferSize);
    HAL_TIM_Base_Start(&htim6);�?�?

    This in TIM6 setup

    htim6.Instance = TIM6;
    htim6.Init.Prescaler = 1;
    htim6.Init.CounterMode = TIM_COUNTERMODE_UP;
    htim6.Init.Period = 2250;
    htim6.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;
    ...
    sMasterConfig.MasterOutputTrigger = TIM_TRGO_UPDATE;
    sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;�?�?�?�?�?�?�?�?�?�?

    This is ADC1 setup

     hadc1.Instance = ADC1;
     hadc1.Init.ClockPrescaler = ADC_CLOCK_SYNC_PCLK_DIV4;
     hadc1.Init.Resolution = ADC_RESOLUTION_12B;
     hadc1.Init.ScanConvMode = DISABLE;
     hadc1.Init.ContinuousConvMode = DISABLE;
     hadc1.Init.DiscontinuousConvMode = DISABLE;
     hadc1.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_RISING;
     hadc1.Init.ExternalTrigConv = ADC_EXTERNALTRIGCONV_T6_TRGO;
     hadc1.Init.DataAlign = ADC_DATAALIGN_RIGHT;
     hadc1.Init.NbrOfConversion = 1;
     hadc1.Init.DMAContinuousRequests = DISABLE;
     hadc1.Init.EOCSelection = ADC_EOC_SINGLE_CONV;�?�?�?�?�?�?�?�?�?�?�?�?