Question
DMA UART TX single transfer
Hello, I have an stm32F103, I would like to start using DMA to transfer data from memory to TX pin, in circular mode it works fine but when I switch to normal mode it works only once, I cannot use the debug function since I'm not using a ST-Link, so here is the main code:
int main(void)
{
/* USER CODE BEGIN 1 */
uint8_t TX[4] = { 97, 98, 99, 10 };
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_DMA_Init();
MX_I2C1_Init();
MX_USART1_UART_Init();
MX_SPI2_Init();
MX_FATFS_Init();
/* USER CODE BEGIN 2 */
HAL_UART_Transmit_DMA(&huart1, TX, 4);
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
HAL_UART_Transmit_DMA(&huart1, TX, 4);
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */
}
static void MX_DMA_Init(void)
{
/* DMA controller clock enable */
__HAL_RCC_DMA1_CLK_ENABLE();
/* DMA interrupt init */
/* DMA1_Channel4_IRQn interrupt configuration */
HAL_NVIC_SetPriority(DMA1_Channel4_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(DMA1_Channel4_IRQn);
/* DMA1_Channel5_IRQn interrupt configuration */
HAL_NVIC_SetPriority(DMA1_Channel5_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(DMA1_Channel5_IRQn);
}I tried every crazy combination, clearing directly registers, using different callback functions, refilling the buffer... the result is the same I only receive the information only at startup then nothing.
Help please :'(