Question
DMA to TIM3 CCR1 problem!
Posted on August 08, 2015 at 05:21
Hi! Device is STM32F103C8
A update event from TIM4 is used to trigger DMA channel7 who then is supposed to transfer 9 values in circular mode to TIM3 CCR1. However the DMA transfers only one value and that one is set to 0 and the rest is set to 127!? So what i get is narrow pulse on CCR1 going round at the speed of TIM4 update event.1.
#include ''stm32f10x.h'' 2. uint8_t buffer[9] = {0,16,32,48,64,80,96,112,127};void tim4(void) { /************************* Tim4 ****************************************************/ TIM4->CCMR1 |= 0b0110000001100000; //OCM1 is set to PWM1 mode and OCM2 is set to PWM1 mode TIM4->CCMR2 |= 0b0110000001100000; //OCM3 is set to PWM1 mode and OCM4 is set to PWM1 mode TIM4->CCER |= TIM_CCER_CC1E; //Capture/Compare 1 output enable TIM4->CCER |= TIM_CCER_CC2E; //Capture/Compare 2 output enable TIM4->CCER |= TIM_CCER_CC3E; //Capture/Compare 1 output enable TIM4->CCER |= TIM_CCER_CC4E; //Capture/Compare 2 output enable TIM4->PSC = 8192; TIM4->ARR = 1; TIM4->CCR1 = 1; //CCR1 register set to initial PWM1 value TIM4->CCR2 = 1; //CCR2 register set to initial PWM2 value TIM4->CCR3 = 1; TIM4->CCR4 = 1; TIM4->DIER |= TIM_DIER_UDE; //DMA request on tim4 Update event TIM4->BDTR |= TIM_BDTR_MOE; //Enable output stage //TIM4->CR2 |= TIM_CR2_CCDS; //DMA request on Update event TIM4->CR1 |= TIM_CR1_CEN; //Enable Timer4 }
void tim3( void ) { /************ Tim3 ********************************************************************/ TIM3->CCMR1 |= 0b0110000001100000; //OCM1 is set to PWM1 mode and OCM2 is set to PWM1 mode TIM3->CCMR2 |= 0b0110000001100000; //OCM3 is set to PWM1 mode and OCM4 is set to PMW1 mode TIM3->CCER |= TIM_CCER_CC1E; //Capture/Compare 1 output enable TIM3->CCER |= TIM_CCER_CC2E; //Capture/Compare 2 output enable TIM3->CCER |= TIM_CCER_CC3E; //Capture/Compare 3 output enable TIM3->CCER |= TIM_CCER_CC4E; //Capture/Compare 4 output enable TIM3->PSC = 0; TIM3->ARR = 127; TIM3->CCR1 = 64; //CCR1 register set to initial PWM1 value TIM3->CCR2 = 64; //CCR2 register set to initial PWM2 value TIM3->CCR3 = 64;<br> TIM3->CCR4 = 64;<br> TIM3->BDTR |= TIM_BDTR_MOE; //Enable output stage TIM3->CR1 |= TIM_CR1_CEN; //Enable Timer3 }
void dma1( void ) { /**************** DMA configuration......DMA ch7 triggered by TIM4 UD ***********************************/ DMA1_Channel7->CCR = 0; //Reset CCR DMA1->IFCR = 0; //Clear all pending (old) DMA1 Stream's interrupts DMA1_Channel7->CNDTR = 9; //Number of DMA transfers DMA1_Channel7->CMAR |= (uint32_t)&buffer; //Source, should fetch data from buffer!??! DMA1_Channel7->CPAR |= (uint32_t)&(TIM3->CCR1); //Destination, TIM3 CCR1 //DMA1_Channel7->CCR |= DMA_CCR7_PSIZE_0; //Set peripheral size to 16bits //DMA1_Channel7->CCR |= DMA_CCR7_MSIZE_0; //Set memory size to 16bits DMA1_Channel7->CCR |= DMA_CCR7_DIR; //Read from memory to peripheral DMA1_Channel7->CCR |= DMA_CCR7_MINC; //Memory increment enabled //DMA1_Channel7->CCR |= DMA_CCR7_MEM2MEM; //Memory to memory enabled //DMA1_Channel7->CCR |= DMA_CCR7_PINC; //Peripheral increment enabled DMA1_Channel7->CCR |= DMA_CCR7_CIRC; //DMA set to circular mode DMA1_Channel7->CCR |= DMA_CCR7_PL; //Channel Priority level set to very high DMA1_Channel7->CCR |= DMA_CCR7_EN; //DMA channel7 enabled }