Question
DMA to external DAC transfer via SPI communication
Posted on November 13, 2014 at 13:32
Hi everybody,
I'm a beginner with STM32F30x µP. I'd like to made a DMA transfers from SRAM to an external DAC via SPI communication. Is it possible? Can I even configure a timer (TIMx) to generate a PWM signal or One Pulse Mode signal on TIMx_CHx and use it as DMA trigger and also as NSS signal input to latch the SPI data transfers to my external DAC? Thanks for your advice on that point. Regards, Franck