Skip to main content
abhishek2
Associate II
August 18, 2008
Question

DMA pheripheral transfer example

  • August 18, 2008
  • 2 replies
  • 682 views
Posted on August 18, 2008 at 09:45

DMA pheripheral transfer example

    This topic has been closed for replies.

    2 replies

    16-32micros
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:42

    Hi,

    May this link helps you :

    http://www.st.com/mcu/forums-cat-7180-23.html

    Cheers,

    STOne-32.

    abhishek2
    abhishek2Author
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 12:42

    HEllo everybody

    I am stuck with building the DMA example 4 in which the ADC (pot in STM3210B-EVAL board) is configured to generate PWM pulses at the output (PA08) through the DMA channel5. I am able to build the project and even download it into the flash. Unfortunately I do not see any change in the Oscilloscope. The debug does not end with highligting the int main function which usually happens with other examples. Only ''break'' and ''stop debugging'' buttons are active and others are inactive in IAR.

    Thanking you

    AR