Skip to main content
Uwe Bonnes
Chief
Jul 6, 2018 9:29 AM UTC
Question

DMA MEN2MEN and DMAMUX

Posted on July 06, 2018 at 11:29

Hello,

is the DMAMUX somehow involved when doing DMA MEM2MEM transfers? Is the value in the DMAMUX channel corresponding to the selectedMEM2MEM DMA channel irrelevant or must it be zero? I did not see MEM2MEN mentioned in the DMAMUX chapter of RM0432.

    This topic has been closed for replies.

    1 reply

    ST Technical Moderator
    Jul 9, 2018 3:29 PM UTC
    Posted on July 09, 2018 at 17:29

    Hello

    Bonnes.Uwe

     ,

    DMAMUX is only for peripherals and not memory to memory.

    When a channel of DMA1 is programmed with DMA_CCRx.MEM2MEM=1, there is no hardware peripheral request.

    So,

     DMAMUX is not involved. 

    With Regards,

    Imen

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks