Skip to main content
jmiguelg
Associate
July 21, 2015
Question

DMA data from ADC does not refresh

  • July 21, 2015
  • 1 reply
  • 654 views
Posted on July 21, 2015 at 14:44

Hello all,

I am writing an application on a STM32F4 which reads from two sensors. I do it with two ADC3 channels with DMA. I use HAL_DRIVERS

I write on a buffer several readings from three sensors by calling:

HAL_ADC_Start(&hadc3);

HAL_ADC_Start_DMA(&hadc3, (uint32_t*)ADC1ConvertedValues, 18);

In ''void HAL_ADC_ConvCpltCallback(ADC_HandleTypeDef* hadc)''

I call: HAL_ADC_Stop_DMA(&hadc3);

and then HAL_ADC_Start_DMA(&hadc3, (uint32_t*)ADC1ConvertedValues, 18);

when I need another sensor reading.

The problem is that ADC1ConvertedValues[] has always the same information (only the first readings are ok). The others make no effect in ADC1ConvertedValues[].

Any idea why?

Many thanks in advance.

Some code of important functions:

void MX_ADC3_Init(void)

{

  ADC_ChannelConfTypeDef sConfig;

    /**Configure the global features of the ADC (Clock, Resolution, Data Alignment and number of conversion) 

    */

  hadc3.Instance = ADC3;

  hadc3.Init.ClockPrescaler = ADC_CLOCKPRESCALER_PCLK_DIV2;

  hadc3.Init.Resolution = ADC_RESOLUTION12b;

  hadc3.Init.ScanConvMode = ENABLE;

  hadc3.Init.ContinuousConvMode = ENABLE;

  hadc3.Init.DiscontinuousConvMode = DISABLE;

  hadc3.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE;

  hadc3.Init.DataAlign = ADC_DATAALIGN_RIGHT;

  hadc3.Init.NbrOfConversion = 3;

  hadc3.Init.DMAContinuousRequests = DISABLE;

  hadc3.Init.EOCSelection = EOC_SINGLE_CONV;

  HAL_ADC_Init(&hadc3);

    /**Configure for the selected ADC regular channel its corresponding rank in the sequencer and its sample time. 

    */

  sConfig.Channel = ADC_CHANNEL_9;

  sConfig.Rank = 1;

  sConfig.SamplingTime = ADC_SAMPLETIME_15CYCLES;

  HAL_ADC_ConfigChannel(&hadc3, &sConfig);

    /**Configure for the selected ADC regular channel its corresponding rank in the sequencer and its sample time. 

    */

  sConfig.Channel = ADC_CHANNEL_14;

  sConfig.Rank = 2;

  HAL_ADC_ConfigChannel(&hadc3, &sConfig);

    /**Configure for the selected ADC regular channel its corresponding rank in the sequencer and its sample time. 

    */

  sConfig.Channel = ADC_CHANNEL_15;

  sConfig.Rank = 3;

  HAL_ADC_ConfigChannel(&hadc3, &sConfig);

}

void HAL_ADC_MspInit(ADC_HandleTypeDef* hadc)

{

  GPIO_InitTypeDef GPIO_InitStruct;

  if(hadc->Instance==ADC3)

  {

  /* USER CODE BEGIN ADC3_MspInit 0 */

  /* USER CODE END ADC3_MspInit 0 */

    /* Peripheral clock enable */

    __ADC3_CLK_ENABLE();

  

    /**ADC3 GPIO Configuration    

    PF3     ------> ADC3_IN9

    PF4     ------> ADC3_IN14

    PF5     ------> ADC3_IN15 

    */

    GPIO_InitStruct.Pin = GPIO_PIN_3|GPIO_PIN_4|GPIO_PIN_5;

    GPIO_InitStruct.Mode = GPIO_MODE_ANALOG;

    GPIO_InitStruct.Pull = GPIO_NOPULL;

    HAL_GPIO_Init(GPIOF, &GPIO_InitStruct);

    /* Peripheral DMA init*/

  

    hdma_adc3.Instance = DMA2_Stream0;

    hdma_adc3.Init.Channel = DMA_CHANNEL_2;

    hdma_adc3.Init.Direction = DMA_PERIPH_TO_MEMORY;

    hdma_adc3.Init.PeriphInc = DMA_PINC_DISABLE;

    hdma_adc3.Init.MemInc = DMA_MINC_ENABLE;

    hdma_adc3.Init.PeriphDataAlignment = DMA_PDATAALIGN_WORD;

    hdma_adc3.Init.MemDataAlignment = DMA_MDATAALIGN_WORD;

    hdma_adc3.Init.Mode = DMA_CIRCULAR;

    hdma_adc3.Init.Priority = DMA_PRIORITY_MEDIUM;

    hdma_adc3.Init.FIFOMode = DMA_FIFOMODE_DISABLE;

    HAL_DMA_Init(&hdma_adc3);

    __HAL_LINKDMA(hadc,DMA_Handle,hdma_adc3);

  /* USER CODE BEGIN ADC3_MspInit 1 */

  /* USER CODE END ADC3_MspInit 1 */

  }

}

#stm32f4 #adc #dma
This topic has been closed for replies.

1 reply

jmiguelg
jmiguelgAuthor
Associate
July 22, 2015
Posted on July 22, 2015 at 09:00

Hello,

The problem is that after HAL_ADC_Stop_DMA is executed in

void HAL_ADC_ConvCpltCallback(ADC_HandleTypeDef* hadc)

{

HAL_ADC_Stop_DMA(&hadc3);

}

next calls to HAL_ADC_Start_DMA(&hadc3, (uint32_t*)ADC1ConvertedValues, 18);

do not fire the ADC/DMA work so that the interrupt HAL_ADC_ConvCpltCallback is never called again.

Any idea why ?

Best Regards,

Jorge