Question
DMA and two or more U(S)ARTs
Posted on October 03, 2013 at 09:50
Can I configure two usart's to use one DMA? In datasheet there is table called ''DMAx request mapping'' and for stm32f40/1/2/3 eg. UART4 uses
channel 4 for RX and TX DMA trigger on stream 2 and 4. Can I configure stream 0 and 5 to use UART5 (also chanell 4) at the same time or this setting will collide with settings of UART4 DMA ? #stm32-usart-dma