Skip to main content
howard n2wx
Associate III
Feb 7, 2017 9:02 PM UTC
Solved

Discovery board with STM32F417?

Posted on February 07, 2017 at 22:02

Is a discovery board available for any of the stm32f417 variants?

#stm32f417 #stm32f4-discovery
This topic has been closed for replies.
waclawek.jan
waclawek.janBest answer
Super User
Feb 7, 2017 9:34 PM UTC
Posted on February 07, 2017 at 22:34

None I know of.

The only dedicated devboard I know of is the related

http://www.st.com/en/evaluation-tools/stm3241g-eval.html

, but it's a bit pricey, hundreds of $.

In fact, I know of none of the DISCOs or NUCLEOs populated with any of the crypto-enabled STM32 variants.

The 'F417 is the same as 'F407, so as far as the peripherals are concerned, you can fully asses them with the '

http://www.st.com/content/st_com/en/products/evaluation-tools/product-evaluation-tools/mcu-eval-tools/stm32-mcu-eval-tools/stm32-mcu-discovery-kits/stm32f4discovery.html

.

If you want to play specifically with the 'F417's crypto features, then one of the options is to buy either the 'F4 DISCO or any Nucleo144, plus a 'F417 in matching package, and swap it for what is on the board.

JW

4 replies

waclawek.jan
waclawek.janBest answer
Super User
Feb 7, 2017 9:34 PM UTC
Posted on February 07, 2017 at 22:34

None I know of.

The only dedicated devboard I know of is the related

http://www.st.com/en/evaluation-tools/stm3241g-eval.html

, but it's a bit pricey, hundreds of $.

In fact, I know of none of the DISCOs or NUCLEOs populated with any of the crypto-enabled STM32 variants.

The 'F417 is the same as 'F407, so as far as the peripherals are concerned, you can fully asses them with the '

http://www.st.com/content/st_com/en/products/evaluation-tools/product-evaluation-tools/mcu-eval-tools/stm32-mcu-eval-tools/stm32-mcu-discovery-kits/stm32f4discovery.html

.

If you want to play specifically with the 'F417's crypto features, then one of the options is to buy either the 'F4 DISCO or any Nucleo144, plus a 'F417 in matching package, and swap it for what is on the board.

JW

howard n2wx
Associate III
Feb 7, 2017 10:47 PM UTC
Posted on February 07, 2017 at 22:47

waclawek.jan wrote:

...

If you want to play specifically with the 'F417's crypto features, then one of the options is to buy either the 'F4 DISCO or any Nucleo144, plus a 'F417 in matching package, and swap it for what is on the board.

JW

Absent the disco for the 417 this is what I'll do.   Thanks!

Tesla DeLorean
Guru
Feb 7, 2017 10:29 PM UTC
Posted on February 07, 2017 at 23:29

Mikroe has a number of boards with crypto chips.

https://shop.mikroe.com/development-boards/starter/clicker/stm32f4

 

Others have swapped parts on the DISCO, and I've populated my own boards with sample parts.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
howard n2wx
Associate III
Feb 7, 2017 11:43 PM UTC
Posted on February 07, 2017 at 23:43

Clive One wrote:

Mikroe has a number of boards with crypto chips.

/external-link.jspa?url=https%3A%2F%2Fshop.mikroe.com%2Fdevelopment-boards%2Fstarter%2Fclicker%2Fstm32f4

Others have swapped parts on the DISCO, and I've populated my own boards with sample parts.

Thank you for the vector. Mikroe has cool stuff! I wish I didn't need ethernet connectivity and crypto