directly read register status instead of HAL_GPIO_Readpin();
i am trying to bit bang 14 bits grey code. my output is not steady
uint16_t readbits(uint16_t dataPin, uint16_t clockPin) {
uint16_t value =0;
for (int i = 0; i <14; ++i) {
value <<= 1;
HAL_GPIO_WritePin(GPIOC, clockPin, GPIO_PIN_RESET);
delay_us(20);
HAL_GPIO_WritePin(GPIOC, clockPin, GPIO_PIN_SET);
delay_us(20);
value |= HAL_GPIO_ReadPin(GPIOC, dataPin);
}
return value;
}
i think HAL_GPIO_ReadPin is not fast enough
in the while loop ()
DATA1 = readbits(DATA1_L_Pin, CLK_SSI_PORT_Pin);
how can change HAL_GPIO_ReadPin(GPIOC, GPIO_PIN_2); for example to read register status?