Question
digital sampling of GPIO
Posted on May 26, 2013 at 00:35
Hi,
is it possible to sample GPIOA Bit7-0 into SRAM as byte and to have kind of ''Clk'' nonPWM output on other GPIO , with higher speed than 20MHz on STM32F103 72MHz ? this gives me 10MHz clk output on PC2: Buffer_ptr=(uint8_t *)Buffer; while( 1 ) { *(Buffer_ptr++)=(uint8_t)GPIOA->IDR; GPIOC->ODR = GPIO_Pin_2; if(Buffer_ptr>=(uint8_t *)(Buffer+20000)) break; GPIOC->ODR = 0; } Thank You for all replies