Skip to main content
ASiva.1
Associate III
Jun 12, 2025 6:26 PM UTC
Question

Digital Input Wrong value

I have done a PCB Design with microcontroller STM32L071CZT6 as the mcu. PB15 which is a 5V tolerant pin is connected to a source of 4.9 V with a resistor 270 kOhm in between. I measured the voltage at the PB15 pin to be 4.9 V but, when I set it as Digital Input pin with no pull it does not read HIGH. But, I remember the previous batch of boards with the same design had this pin read HIGH by the same firmware.

This topic has been closed for replies.

2 replies

KnarfB
Super User
Jun 12, 2025 6:56 PM UTC

Dump the GPIOB register values to double check correct settings. 

The data sheet says:  Input voltage on FT and FTf pins max. VDD+4.0, so applying 5V is illegal while the MCU is not powered. Can this be excluded?

hth

KnarfB

TDK
Jun 12, 2025 7:28 PM UTC

Related/duplicate?

STM32L071CBT6 issue While recieving Input for GPIO... - STMicroelectronics Community

 

Just a coincidence that you are both asking about PB15 input not reading high at 5V on the same chip?

"If you feel a post has answered your question, please click ""Accept as Solution""."