Visitor II
May 15, 2012
Question
Difficuly of implementing nand driver on STM32F205ZG
- May 15, 2012
- 2 replies
- 1194 views
Posted on May 15, 2012 at 08:47
Hi all,
Now, I'm trying to implement nand driver of SAMSUNG K9K8G08U0D (SLC, 1GBYTE) on STM32F205ZG cpu. However, it not easy to do it. First, reading device ID is OK. Second, block erase function is also OK. But, read & write operation is not OK. For example, If I write 0x66 all in one page (2048Byte) and check it has been saved ok, data may be randomly saved. Moreover, If I read erased page, first 2 or 3 bytes are ''0x30'' or ''0x33'' and remaing bytes are all ''0xFF''. I also have hard time to set parameters below. I tried to find values for parameter refering to AN2784 and applied to them but It didn't work well, either. p.FSMC_SetupTime = 32;//12;//1; p.FSMC_WaitSetupTime = 64;//64;//15;//3; p.FSMC_HoldSetupTime = 48;//48;//12;//2; p.FSMC_HiZSetupTime = 32;//24;//3;//1; If you have a tip, please answer. Thanks.