Skip to main content
J.Bepler
Associate
October 26, 2022
Solved

Differences between the Nucleo-144 STM32H743ZI2 and STM32H743ZI

I'm stuck trying to understand the differences between the two Nucleo-144 boards

STM32H743ZI (seems to be the older version but with lots of resources but outdated)

and

STM32H743ZI2 (current version but i can hardly find working examples and resources)

can someone point me in the right direction?

why do some examples designed for the ZI not work on the ZI2 ?

where exactly are the diferences, at first glance they seem identical.

This topic has been closed for replies.
Tesla DeLorean
Tesla DeLoreanBest answer
Guru
October 26, 2022

Related defines, check stm32h7xx_nucleo_conf.h

USE_HAL_DRIVER, STM32H743xx, USE_NUCLEO_144

USE_NUCLEO_H743ZI

USE_NUCLEO_H743ZI2

LED2

PB7 BLUE (ZI)

PE1 YELLOW (ZI2)

ARDUINO D4

PF14 (ZI)

PE14 (ZI2)

ARDUINO D8

PG9 (ZI)

PF3 (ZI2)

PE2 QSPI/SAI CONFLICTED

PB13 SAI/ETHERNET CONFLICTED

PA7 D11/ETHERNET CONFLICTED

QSPI CS

PB6 (ZI)

PG6 (ZI2) or PB6 will SB made

Read the notes and solder-bridge options/defaults

MB1137 UM1974 (ZI)

https://www.st.com/resource/en/user_manual/um1974-stm32-nucleo144-boards-mb1137-stmicroelectronics.pdf

https://www.st.com/resource/en/schematic_pack/nucleo_144pins_sch.zip

MB1364 UM2407 (ZI2)

https://www.st.com/resource/en/user_manual/dm00499160-stm32h7-nucleo144-boards-mb1364-stmicroelectronics.pdf

https://www.st.com/content/ccc/resource/technical/layouts_and_diagrams/schematic_pack/group1/79/99/be/65/3c/76/40/d6/MB1364-H743ZI-C01_Schematic/files/MB1364-H743ZI-C01_Schematic.pdf/jcr:content/translations/en.MB1364-H743ZI-C01_Schematic.pdf

https://paypal.me/cliveone

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..

5 replies

Tesla DeLorean
Guru
October 26, 2022

Handful of pins related to LEDs, QSPI and ETHERNET, as I recall, reducing/removing some potential stubs. Solder Bridges and default usage expectations.

​

Different HSE clock furnished by ST-LINK/V3​

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
J.Bepler
J.BeplerAuthor
Associate
October 26, 2022

could you go ito detail about the ethernet pins particularly? where did you find documentation that explains that?

Tesla DeLorean
Guru
October 26, 2022

I went through the manual and schematic whilst porting some QSPI support.

Perhaps start by looking at the MORPHO​ connector.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
ST Technical Moderator
October 26, 2022

Please check DB3171 for more details.

You can also check the user manual UM2407 and board reference MB1364

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL