Skip to main content
SSchi.4
Associate
July 28, 2022
Solved

Difference of writing 0xFFFFFFFFFFFFFFFF to page erase in flash?

Hi,

After a flash page erase I can write 0xFFFFFFFFFFFFFFFF to a certain position in my desired page (see code snippet). This for sure doesn't change the content of my Flash. However if I want to write again on that very same position, a PROGERR comes up. So there must be a bit or so that describes if a position in the flash page has already been written or not (even if it is a 0xFFFFFFFFFFFFFFFF value). Where can I find that bit?

HAL_FLASH_Unlock();
 if (HAL_FLASH_Program(FLASH_TYPEPROGRAM_DOUBLEWORD, 0x0801F000, 0xFFFFFFFFFFFFFFFF) != HAL_OK)
 {
 Error_Handler();
 }
 HAL_FLASH_Lock();
 
 HAL_FLASH_Unlock();
 if (HAL_FLASH_Program(FLASH_TYPEPROGRAM_DOUBLEWORD, 0x0801F000, 0x1111111111111111) != HAL_OK)
 {
 Error_Handler(); // This Error_Handler() gets called, due to PROGERR
 }
 HAL_FLASH_Lock();

Kind regards

Simon

This topic has been closed for replies.
Tesla DeLorean
Tesla DeLoreanBest answer
Guru
July 28, 2022

You get ONE bite of the apple, you can't do this BIT KNOCK DOWN thing you might have used elsewhere. Only write a value to memory if it's different to the current/initial content.

The flash lines have ECC bits that aren't visible to you.

Other flash devices can be multi-level, ie not binary, so your methods/expectation might need to change/evolve.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..

7 replies

Uwe Bonnes
Chief
July 28, 2022

After erase, ECC is cleared. After writing the erased pattern, ECC is set to some other value and so a second write can not set the right ECC.

SSchi.4
SSchi.4Author
Associate
July 28, 2022

Thanks for the quick response, however I cannot detect any changes in ECC for both writes. ECC remains 0x0 the whole writing process.

Tesla DeLorean
Tesla DeLoreanBest answer
Guru
July 28, 2022

You get ONE bite of the apple, you can't do this BIT KNOCK DOWN thing you might have used elsewhere. Only write a value to memory if it's different to the current/initial content.

The flash lines have ECC bits that aren't visible to you.

Other flash devices can be multi-level, ie not binary, so your methods/expectation might need to change/evolve.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
SSchi.4
SSchi.4Author
Associate
July 28, 2022

alright, thanks for clearification. Then I have to find a workaround

Tesla DeLorean
Guru
July 28, 2022

Yes its unfortunate, as it gets to be expensive. Perhaps the 64-bit write can hold other data as you journal it.

Some of the other parts have some actual EEPROM

The width comes from the methods used to overcome the inherent slowness of reliable FLASH, perhaps probably still 35ns or so, the width allows for prefetching, buffering or caching to spread the cost of access over multiple words. Basically 0-cycle, and faster than 1-cycle RAM, or adding in wait-states.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Pavel A.
July 29, 2022

It seems to be a well known fact that internal flash of STM32s can be written only once after erase.

Even if you write FF bytes over erased space that reads FF.

Not sure whether it is effect of internal ECC or not.

Bottom line, it isn't possible to leave a FF-filled "hole" in the binary and write to it later (unless you have a custom flash utility that deliberately skips areas of FFs).

Space from the end of firmware image to the end of erase block usually remains writable.

Piranha
Principal III
July 29, 2022

On F2/F4/F7 and probably some other series the flash can be written as many times as necessary, but the bits are only flipping from 1 to 0.