Skip to main content
waldin80
Associate III
July 28, 2010
Question

Difference between Low/medium/high density devices and conectivity line devices

  • July 28, 2010
  • 4 replies
  • 2340 views
Posted on July 28, 2010 at 08:57

Difference between Low/medium/high density devices and conectivity line devices

    This topic has been closed for replies.

    4 replies

    waldin80
    waldin80Author
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 14:00

    Thks for replying:

    My doubt is, what kind of type of device I have?

    I´m programming STM32F103VE.

    Is it High density device or Connectivity device?

    Both groups of devices have diferent clock tree (see RM0008 pag 77 and 107), that is my doubt

    stforum2
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 14:00

    A brief description of each sub-family is listed here:

    http://www.st.com/mcu/familiesdocs-110.html#Datasheet

    but if you really want to know the detailed differences then you need to download each datasheet.

    The 'density' directly relates to the amount of flash memory.

    'connectivity line' has an OTG USB interface, dual CAN interfaces and ethernet

    'performance line' has CAN and USB (device)

    'USB access line' has USB but no CAN

    'access line' has neither USB or CAN

    'value line' has an HDMI interface

    Hope this helps.

    stforum2
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 14:00

    You have a high density performance device with 512k of flash and 64k of RAM.

    14611.pdf describes your device.

    Connectivity devices are ...105... and ...107...

    waldin80
    waldin80Author
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 14:00

    Ok, Thks for the help. Ten points for you 0690X0000060MlFQAU.gif