Skip to main content

3 replies

Amel NASRI
ST Technical Moderator
Sep 9, 2026 2:20 PM UTC

Hi ​@waclawek.jan,

I'll say it is not a wrong information in st.com, but I don't have much more details to share right now.

If I have more information, we (me or other colleagues) will come back here.

-Amel

To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.
Andrew Neil
Super User
Sep 9, 2026 2:40 PM UTC

Trying to rationalise packaging?

I imagine that QFP becomes problematic at very high pin counts - due to getting enough “circumference” to fit all those pins?

So anything >176 pins is now only in grid-type packages ?

 

PS:

https://en.wikipedia.org/wiki/Quad_flat_package#Limitations

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
waclawek.jan
Super User
Sep 10, 2026 8:20 AM UTC

Well, these are models which are already out there, fully qualified, mass produced; not “future product/proposal, which turned out to be unrealistic”.

ST had only a single vendor for this particular package, and they have withdrawn. The last-buy date for the above listed products is next year.

So the real question here is, what’s the value of ST’s 10-year promise, then. We’ve seen ST fiddling with that in the past and credit is so hard to build and so easy to lose. What happens if the packaging vendor stops providing e.g. the LQFP176?

Btw. ST does have their own in-house packaging, except not for the larger QFPs. At the moment.

JW