Question
Did I break my 407 with +5V?
Posted on June 26, 2018 at 01:12
I accidentally used a 5V regulator instead of 3.3V. After fixing that the SWD dongle/ST link says no connection to target. This happens to be my only prototype now. Building a new or swapping the 100pin STM32F407 isn't fun. Has anyone experience of this kind of situation. The absolute maximum VDD is 4.0V.
I have checked SWD connections and Boot0 is pulled low.