Skip to main content
Pedram
Associate III
February 4, 2018
Question

Determine STM32 reset source with HAL

  • February 4, 2018
  • 2 replies
  • 3089 views
Posted on February 04, 2018 at 12:15

Hello friends

How can Determine STM32 reset source with HAL ?

STM32F407ZET6

Thanks

    This topic has been closed for replies.

    2 replies

    Tesla DeLorean
    Guru
    February 4, 2018
    Posted on February 04, 2018 at 15:05

      /* Enable Power Clock */

      __HAL_RCC_PWR_CLK_ENABLE();

      /* Check and Clear the Wakeup flag */

      if(__HAL_PWR_GET_FLAG(PWR_FLAG_WU) != RESET)

      {

        __HAL_PWR_CLEAR_FLAG(PWR_FLAG_WU);

      }

      /* Check if the system was resumed from StandBy mode */

      if(__HAL_PWR_GET_FLAG(PWR_FLAG_SB) != RESET)

      {

        /* Clear StandBy flag */

        __HAL_PWR_CLEAR_FLAG(PWR_FLAG_SB);

    }

      {

        /* Check if the Power On Reset flag is set */

        if (__HAL_RCC_GET_FLAG(RCC_FLAG_PORRST) != RESET)

        {

          /* Turn on LED1: Power on reset occurred */

          BSP_LED_On(LED1);

        }

        /* Check if Pin Reset flag is set */

        if (__HAL_RCC_GET_FLAG(RCC_FLAG_PINRST) != RESET)

        {

          /* Turn on LED1: External reset occurred */

          BSP_LED_On(LED1);

        }

        /* Clear source Reset Flag */

        __HAL_RCC_CLEAR_RESET_FLAGS();

      }
    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    rm2399
    Associate II
    February 4, 2018
    Posted on February 04, 2018 at 15:07

    Find the information in stm32f4xx_hal_rcc.h at line 1227ff

    /** @brief  Check RCC flag is set or not.

      * @param  __FLAG__ specifies the flag to check.

      *         This parameter can be one of the following values:

      *            @arg RCC_FLAG_HSIRDY: HSI oscillator clock ready.

      *            @arg RCC_FLAG_HSERDY: HSE oscillator clock ready.

      *            @arg RCC_FLAG_PLLRDY: Main PLL clock ready.

      *            @arg RCC_FLAG_PLLI2SRDY: PLLI2S clock ready.

      *            @arg RCC_FLAG_LSERDY: LSE oscillator clock ready.

      *            @arg RCC_FLAG_LSIRDY: LSI oscillator clock ready.

      *            @arg RCC_FLAG_BORRST: POR/PDR or BOR reset.

      *            @arg RCC_FLAG_PINRST: Pin reset.

      *            @arg RCC_FLAG_PORRST: POR/PDR reset.

      *            @arg RCC_FLAG_SFTRST: Software reset.

      *            @arg RCC_FLAG_IWDGRST: Independent Watchdog reset.

      *            @arg RCC_FLAG_WWDGRST: Window Watchdog reset.

      *            @arg RCC_FLAG_LPWRRST: Low Power reset.

      * @retval The new state of __FLAG__ (TRUE or FALSE).

      */

    #define RCC_FLAG_MASK  ((uint8_t)0x1FU)

    #define __HAL_RCC_GET_FLAG(__FLAG__) (((((((__FLAG__) >> 5U) == 1U)? RCC->CR :((((__FLAG__) >> 5U) == 2U) ? RCC->BDCR :((((__FLAG__) >> 5U) == 3U)? RCC->CSR :RCC->CIR))) & (1U << ((__FLAG__) & RCC_FLAG_MASK)))!= 0U)? 1U : 0U)