Skip to main content
Roibert
Associate II
April 23, 2024
Question

Delay in SPI Transfer with STM32H7

Dear Forum

Im using STM32 H755 ZI in the starter kit.

 

I set the Timer 4 for generate a Interrupt each 1ms.

At begin of INT:

     -I toggle a PIN,

      -and, send a SPI data (8 byte or 16..not important)

What I noted is a delay of almost 10uS beetwen pin toggle and begin of 1st bit TX from

SPI (begin of SPI transmission i means)

Some data:

FCPU=64M coming from internal 64M HSI

SPI1_CLK=4M coming from PER_CLK =64M  (with SPI prescaler=16  -->4M) 

FAPB=64M

Code inside INT Timer:

HAL_GPIO_TogglePin(PF10Test_GPIO_Port, PF10Test_Pin);

HAL_SPI_Transmit(&hspi1, p_Data16b, 1, 100);

__HAL_TIM_CLEAR_FLAG(htim4, TIM_FLAG_UPDATE);

 

Thanks for your help

Roberto

This topic has been closed for replies.

13 replies

Roibert
RoibertAuthor
Associate II
June 12, 2024

Dear Forum

I modify the freq of CPU and SPI, and get to the conclusion that max distance beetwen 2 consecutive transmisson is circa 1uS (distance bettwen 2 H->L transiction of CS) ; in particular:

- delay decrease if Baud rate increase

-delay decrease if CPU freq incresae.

But this decrease reach a minimun, and then stop (not linear).

Question is what is limiting this disrtance ?

Thanks

Roberto