Skip to main content
timothy
Associate II
July 19, 2013
Question

DELAY help

  • July 19, 2013
  • 4 replies
  • 1062 views
Posted on July 19, 2013 at 07:34

Im trying to create a delay but im lost on how to make one, any code would be great.

-Tim
    This topic has been closed for replies.

    4 replies

    sonurobots
    Associate III
    July 19, 2013
    Posted on July 19, 2013 at 08:24

    just call Delay(500);

    void Delay(int count)

    {

    while(count--);

    }

    if you want some precise delay then go for timers .that's why they are made for .
    zzdz2
    Associate
    July 19, 2013
    Posted on July 19, 2013 at 08:58

    #define TICKSGN ((SysTick_VAL_CURRENT_Msk+1)>>1)
    #define WAITMAX (SysTick_VAL_CURRENT_Msk >> 1)
    static inline void waittick(uint32_t step)
    {
    static uint32_t tick0;
    if (!step)
    {
    tick0 = SysTick->VAL;
    return;
    }
    tick0 -= step;
    while ((tick0 - SysTick->VAL) & TICKSGN)
    {
    __NOP();
    __NOP();
    }
    }
    static inline void sleep(uint32_t delay)
    {
    waittick(0);
    delay++;
    while (delay > WAITMAX)
    {
    waittick(WAITMAX);
    delay -= WAITMAX;
    }
    waittick(delay);
    }

    haythem
    Associate III
    March 18, 2014
    Posted on March 18, 2014 at 22:47

    How can I use the delay function in U.S.

    francescatodiego
    Associate III
    March 19, 2014
    Posted on March 19, 2014 at 02:09

    My hw delay routine

    #include <
    stdbool.h
    >
    #include <
    stdint.h
    >
    #include ''stm32f4xx.h''
    #include ''LIBhwtmr.h''
    #define TIMER_HW_FREQ 1000000 // 1MHz
    // default config APB1clock=Coreclock/4 -> APB1timerclock=2*APB1clock=Coreclock/2
    ///////////////////////////////////////////////////////////////////////////////////////////////
    bool Timer_HW_delay_set (uint32_t time)
    {
    TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure;
    uint32_t PrescalerFreq = TIMER_HW_FREQ ;
    uint32_t PrescalerValue = 0 ;
    uint32_t PresetValue = time ;
    while ((PresetValue >= 0x00010000) && (PrescalerFreq > 0))
    {
    PresetValue >>= 1 ;
    PrescalerFreq >>= 1 ;
    }
    if (PrescalerFreq > 0)
    {
    PrescalerValue = ((SystemCoreClock / 2) / PrescalerFreq) - 1;
    if ((PresetValue < 0x00010000) && (PrescalerValue < 0x00010000))
    {
    RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM6, ENABLE);
    TIM_TimeBaseStructure.TIM_Period = (uint16_t) PresetValue ;
    TIM_TimeBaseStructure.TIM_Prescaler = (uint16_t) PrescalerValue ;
    TIM_TimeBaseStructure.TIM_ClockDivision = 0;
    TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;
    TIM_TimeBaseInit (TIM6, &TIM_TimeBaseStructure);
    TIM_ClearFlag (TIM6, TIM_FLAG_Update) ;
    TIM_Cmd(TIM6, ENABLE);
    return true ;
    }
    }
    return false ;
    }
    ///////////////////////////////////////////////////////////////////////////////////////////////
    bool Timer_HW_expired ()
    {
    return (bool) (TIM_GetFlagStatus(TIM6, TIM_FLAG_Update) != RESET) ;
    }
    ///////////////////////////////////////////////////////////////////////////////////////////////
    void Timer_HW_reset ()
    {
    TIM_Cmd(TIM6, DISABLE);
    RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM6, DISABLE);
    }
    ///////////////////////////////////////////////////////////////////////////////////////////////
    void Timer_HW_wait_delay (uint32_t time)
    {
    Timer_HW_delay_set(time) ;
    while (TIM_GetFlagStatus(TIM6, TIM_FLAG_Update) == RESET) ;
    Timer_HW_reset ()
    }

    You can define the hw timer frequency in TIMER_HW_FREQ define if you use external clock define HSE_VALUE = clock frequency in compiler otherwise SystemCoreClock contain wrong value Delay use TMR6 and if possible use tic 1us (set by define TIMER_HW_FREQ in my code) If delay value > 16bit

    try to

    reduce

    tic frequency and delay until < 16bit and return true if timer start if division fail (very long delay) return false