Skip to main content
flyer31
Senior
Oct 20, 2014 11:06 AM UTC
Question

Decrease priority during runtime of interrupt

Posted on October 20, 2014 at 13:06

Hi,

I have an application where interrupts come very fast on a timer (about 100kHz). Most time this interrupt is handled very immediate, and then all is fine.

This interrupt should have quite high pre-emptive priority, so that it can interrupt also other ''not so important interrupts''.

Just sometimes I want to do some heavier processing also in this fast interrupt. In this case it would be necessary, that I somehow ''decrease the interrupt priority level'' for the running interrupt, and I have to do this WITHIN the interrupt routine (so while the intterupt is running - so that if another higher prio interrupt arrives, it will interrupt this ''heavier processing'').

Is this possible by some register access? Or is it necessary to invoke another software interrupt with lower priority to do the lower priority processing then in this software interrupt?

(register access of course would be very nice, as then I would not loose any processing time for push/pop of registers, also it would be more economic for the stack).
    This topic has been closed for replies.

    3 replies

    chen
    Associate II
    Oct 20, 2014 11:37 AM UTC
    Posted on October 20, 2014 at 13:37

    Hi

    '' it would be necessary, that I somehow ''decrease the interrupt priority level'' for the running interrupt, and I have to do this WITHIN the interrupt routine''

    I believe that this is impossible!

    Once an IRQ triggers and it is executing it's ISR the ARM core hardware has already determined the IRQ and the IRQ level.

    ''Just sometimes I want to do some heavier processing also in this fast interrupt.''

    This appears to be your root cause of your problem.

    Find another way to do the 'processing' outside of the ISR and then get the ISR to pick up the result.

    waclawek.jan
    Super User
    Oct 20, 2014 12:26 PM UTC
    Posted on October 20, 2014 at 14:26

    Read ''Execution priority and priority boosting'' on p.B1-637, in ARMv7-M Architecture

    Reference Manual, ARM DDI 0403D

    JW
    flyer31
    flyer31Author
    Senior
    Oct 20, 2014 6:42 PM UTC
    Posted on October 20, 2014 at 20:42

    Thanks - looking for ''Priority'' in the ARM7 Manual (given in your post): There it describes a special instruction ISB, one of its purposes is ''re-prioritizing the exceptions that have configurable priority'' ... just not stating whether this is inside an interrupt routine.

    Further there is a very promising example ''B1-1'' on page B1-638. I seems to be possible to decrease the Priority (thus increase the priority number) of a running interrupt ... . Just unfortunately this is not the solution for my problem, this would generally decrease the priority of my 100kHz interrupt. I am looking for a way to keep the 100kHz interrupt in ''hot priority'' state, but just somehow decrease the priority of the current ''additional processing stuff'' ... so I think I will have to invoke a sort of software interrupt for this.