Skip to main content
Javierio
Associate II
May 29, 2020 8:48 PM UTC
Question

Debugging/flashing bluepill (stm32f103c8) doable only once??

Hi, im flashing code autogenerated with STM32CUBEMX and using STM32IDE trough an stlink(from a nucleo-F303RE).

The problem: after flashing/debugging the SW pins are left unusable? because i cannot reflash or access the board again unless i manually pull the reseet pin at the same time of flashing.

is there some configuration im doing wrong or some extra wiring i need to take in mind?

the code flashes okay once but is very tyring having to pull the reset every time i flash the bluepill.

thanks in advance for your ideas!

0693W000001pkIqQAI.png0693W000001pkIRQAY.jpg

This topic has been closed for replies.

1 reply

Javierio
JavierioAuthor
Associate II
May 29, 2020 8:51 PM UTC

that was quick.... XD

I realised i was not setting the pins as debugging in stm32cubeMX0693W000001pkJ5QAI.png

now it works flawlessly