Question
Debouncing using registers
Hello, first of all, thanks for all the previous help to everyone. I want to debounce my input, using registers, but I'm running into the issue of it "not working" I am surely missing something in the logic I am overlooking.
here is my interrupt
void Interrupt_Init(void){
EXTI15_10_Init();
NVIC->IP[EXTI15_10_IRQn] = (1 << 4);
NVIC->ISER[40 >> 5] |= (1 << (40 % 32));
}
union InterruptFlag {
struct {
volatile bool flag: 1; // Just one bit for our flag
volatile bool press: 1;
} bits_access;
uint32_t reg; // We'll use this for byte access
};
volatile union InterruptFlag flag = { .bits_access.flag = 0 }; // Initialize to 0
volatile uint16_t pressTime;
volatile bool lastButtonPress=0;
volatile bool buttonPress=1;
void EXTI15_10_IRQHandler(void){
flag.bits_access.flag = !flag.bits_access.flag;
EXTI->PR |= (1<<13); // Clear PR to re-enable EXTI interrupt
}bool debounceButton(){
TIM3->CR1 |= TIM_CR1_CEN;
if((GPIOC->IDR & GPIO_IDR_ID13)!=lastButtonPress){
if(GPIOC->IDR & GPIO_IDR_ID13){
pressTime=TIM3->CNT;
}else{
if(pressTime>10){
flag.bits_access.press=1;
return 1;
}
}
lastButtonPress=GPIOC->IDR & GPIO_IDR_ID13;
}
return 0;
}and above is the debouncing function
and this is what happens in the main function;
while (1)
{
int x;
for(x=0; x<500; x++)
{
if(debounceButton()== 1){
x=x-1;
TIM2->CCR1=x;
}
else{
TIM2->CCR1=x;
delayTRIP(1);
}}
for(x=500; x>0; x--)
{
if(debounceButton()== 1){
x=x+1;
TIM2->CCR1=x;
}
else{
TIM2->CCR1=x;
delayTRIP(1);
}
}
}}]
the button should stop when I press the button for x amount of milliseconds, but whatever I put into the debounce functin doesnt work