Skip to main content
Associate II
May 29, 2025 11:35 AM UTC
Question

Dead Time In General Purpose Timer

I have a doubt about can a general purpose timer generate dead time like advanced timer without changing the duty and frequency is this is possible i tried with center aligned mode but it changes the duty is there is any possiblities??

This topic has been closed for replies.

5 replies

urbito
Senior II
May 29, 2025 12:14 PM UTC

what you can do is to, put a flag, when you want to start the "dead time", and in your timer routine, check for that flag, start counting the death time and then in the place where you said "start dead time", check for the "counting death time" to happen.

 

Hope it helps.

 

greetings

Associate II
May 30, 2025 4:23 AM UTC

I didn't understand what you were exactly saying

TDK
May 29, 2025 12:54 PM UTC

The general purpose timers do not have dead time functionality.

> without changing the duty and frequency

Any modification to the waveform will change one or the other. What exactly are you going for here?

"If you feel a post has answered your question, please click ""Accept as Solution""."
Associate II
May 30, 2025 4:22 AM UTC

I need the same functionality of advanced timer Pwm with dead time same requirements i want in general purpose timer that why i asked is there is any possibility

TDK
May 30, 2025 1:18 PM UTC

No. The dead time feature on advanced timers is not available on general purpose timers.

"If you feel a post has answered your question, please click ""Accept as Solution""."