Question
Dead Time
Posted on October 25, 2010 at 14:28
hi
i am trying to activte TIM1 in complementary mode with dead time. but for some reason i get areverse dead time (both channels are at ''1'' instade of ''0'') why is that i could not find such an option in the manual probebly missed something but what? thanks. #include ''stm32F10x.h'' void setsystemclock(void); int main(void) { setsystemclock(); //set system clock to 24Mhz //rcc configuration RCC->APB2ENR= RCC_APB2ENR_IOPBEN |RCC_APB2ENR_IOPAEN | RCC_APB2ENR_TIM1EN |RCC_APB2ENR_AFIOEN ; //GPIO configuration GPIOB->CRH=0xbb00000;//alternative function output up to 50mhz PB pins 0,1 GPIOA->CRH=0x0bb;//alternative function output up to 50mhz PB pins 0,1 TIM1->ARR=1374; /* Set the Autoreload Register value (Count/f)=(1/(wanted freq))*/ TIM1->EGR=TIM_EGR_UG;/*!<Update Generation */ TIM1->CR2=TIM_CR2_OIS1 ; /*!<Output Idle state 2 (OC2 output) */ TIM1->CCMR1=TIM_CCMR1_OC1M ; /*!<OC1M[2:0] bits (Output Compare 1 Mode) */ TIM1->CCR1=480; /* Set the Capture Compare1 Register value (Duty Cycle)*/ TIM1->CCER=TIM_CCER_CC1E |TIM_CCER_CC1NE | TIM_CCER_CC1P | TIM_CCER_CC1NP ; /*!<Capture/Compare 1 output enable */ TIM1->CCMR1|=TIM_CCMR1_OC1PE ; /*!<Output Compare 1 Preload enable */ TIM1->CR1=TIM_CR1_ARPE; /*!<Auto-reload preload enable */ TIM1->BDTR=TIM_BDTR_OSSR| TIM_BDTR_OSSI | TIM_BDTR_LOCK_0 | 2 | TIM_BDTR_BKE | TIM_BDTR_BKP | TIM_BDTR_AOE; TIM1->CR1=TIM_CR1_CEN; /*!<Counter enable */ TIM1->BDTR=TIM_BDTR_MOE; while(1) { } } void setsystemclock(void) { RCC->CR |= RCC_CR_HSEON; // Wait until it's ready while ((RCC->CR & RCC_CR_HSERDY) == 0) ; // Select PREDIV1 as PLL source and sett PLL mul to 3 (set bit 0) // for 8*3 = 24 MHz RCC->CFGR |= RCC_CFGR_PLLSRC | RCC_CFGR_PLLMULL_0; // Start PLL RCC->CR |= RCC_CR_PLLON; // Wait until it's ready while ((RCC->CR & RCC_CR_PLLRDY) == 0) ; // Select PLL as system clock RCC->CFGR |= RCC_CFGR_SW_PLL; // Here we can check if PLL is used, and maybe disable HSI // Disable HSI RCC->CR &= ~RCC_CR_HSION; RCC->CFGR|=RCC_CFGR_MCO_2; //sys clock output }