Question
dead gpio pins on 4/100 stm32407 chips
Posted on January 07, 2013 at 11:09
i have designed a little pcb which uses a stm32407vet. i have had 100 boards assembled. and 96 of them work great but 4 of them the gpio on 1 pin (different pin each board) is not working) same firmware on each board.
its using the A bank and the gpio goes straight to a 2x7 IDC header on the pcb.have i some how killed the gpio when testing the boards? and zapping it with static by accidently touching the header? how static sensitive is the gpio on these stm32 chips?I cant think what else would effect 4 boards out of 100 batch and kill of random gpio like this?Thanks :)