Question
DCMI to SRAM via DMA does not work
Posted on October 23, 2014 at 11:23
Hello, i have project where i need to capture image from MT9M001 camera, store it inside SRAM (2MB) and do some complex calculation on image.
In order to make it work, i cropped image from 1280x1024 to 1024x1024 so it will fit inside my SRAM, because camera is capable of 10b. I tested SRAM with ST program, where it fills SRAM with data, and checks for errors by reading each number, that works fine, so problem is not inside SRAM config or connections. Since i have scope, i see that after setting camera registers, i get VSYNC, HSYNC, PCLK, and data outputs, no anomaly found by probing So my only cooperate for this problem can be DCMI and DMA config. Can any one spot problems in code ?#define DCMI_DR_ADDRESS (uint32_t)0x50050028
#define FMC_SRAM_ADDRESS (uint32_t)0x64000000
void MT9M001_HW_Init(void)
{
GPIO_InitTypeDef GPIO_InitStructure;
I2C_InitTypeDef I2C_InitStruct;
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA|RCC_AHB1Periph_GPIOB|RCC_AHB1Periph_GPIOC|RCC_AHB1Periph_GPIOE|RCC_AHB1Periph_GPIOG,ENABLE);
GPIO_PinAFConfig(GPIOA, GPIO_PinSource9, GPIO_AF_DCMI); //D0
GPIO_PinAFConfig(GPIOA, GPIO_PinSource10, GPIO_AF_DCMI); //D1
GPIO_PinAFConfig(GPIOG, GPIO_PinSource10, GPIO_AF_DCMI); //D2
GPIO_PinAFConfig(GPIOG, GPIO_PinSource11, GPIO_AF_DCMI); //D3
GPIO_PinAFConfig(GPIOE, GPIO_PinSource4, GPIO_AF_DCMI); //D4
GPIO_PinAFConfig(GPIOB, GPIO_PinSource6, GPIO_AF_DCMI); //D5
GPIO_PinAFConfig(GPIOE, GPIO_PinSource5, GPIO_AF_DCMI); //D6
GPIO_PinAFConfig(GPIOE, GPIO_PinSource6, GPIO_AF_DCMI); //D7
GPIO_PinAFConfig(GPIOC, GPIO_PinSource10, GPIO_AF_DCMI); //D8
GPIO_PinAFConfig(GPIOC, GPIO_PinSource12, GPIO_AF_DCMI); //D9
GPIO_PinAFConfig(GPIOA, GPIO_PinSource4, GPIO_AF_DCMI); //HSYNC
GPIO_PinAFConfig(GPIOB, GPIO_PinSource7, GPIO_AF_DCMI); //VSYNC
GPIO_PinAFConfig(GPIOA, GPIO_PinSource6, GPIO_AF_DCMI); //PCLKX
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_4 | GPIO_Pin_6 | GPIO_Pin_9| GPIO_Pin_10;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP;
GPIO_Init(GPIOA, &GPIO_InitStructure);
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_6 | GPIO_Pin_7;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP;
GPIO_Init(GPIOB, &GPIO_InitStructure);
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_10 | GPIO_Pin_12;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP;
GPIO_Init(GPIOC, &GPIO_InitStructure);
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_4 | GPIO_Pin_5 | GPIO_Pin_6;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP;
GPIO_Init(GPIOE, &GPIO_InitStructure);
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_10 | GPIO_Pin_11;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP;
GPIO_Init(GPIOG, &GPIO_InitStructure);
/* I2C1 clock enable */
RCC_APB1PeriphClockCmd(RCC_APB1Periph_I2C1, ENABLE);
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOB, ENABLE);
GPIO_PinAFConfig(GPIOB, GPIO_PinSource8, GPIO_AF_I2C1);
GPIO_PinAFConfig(GPIOB, GPIO_PinSource9, GPIO_AF_I2C1);
/* Configure I2C1 GPIOs */
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_8 | GPIO_Pin_9;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz;
GPIO_InitStructure.GPIO_OType = GPIO_OType_OD;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
GPIO_Init(GPIOB, &GPIO_InitStructure);
/* Configure I2C1 */
I2C_DeInit(I2C1);
I2C_Cmd(I2C1, ENABLE);
/* Set the I2C structure parameters */
I2C_InitStruct.I2C_Mode = I2C_Mode_I2C;
I2C_InitStruct.I2C_DutyCycle = I2C_DutyCycle_2;
I2C_InitStruct.I2C_OwnAddress1 = 00;
I2C_InitStruct.I2C_Ack = I2C_Ack_Enable;
I2C_InitStruct.I2C_AcknowledgedAddress = I2C_AcknowledgedAddress_7bit;
I2C_InitStruct.I2C_ClockSpeed = 3000;
/* Initialize the I2C peripheral w/ selected parameters */
I2C_Init(I2C1, &I2C_InitStruct);
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_15;//MT9M001 Reset
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_OUT;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP;
GPIO_Init(GPIOA, &GPIO_InitStructure);
}
void MT9M001_Init(void)
{
DCMI_InitTypeDef DCMI_InitStructure;
DMA_InitTypeDef DMA_InitStructure;
/*** Configures the DCMI to interface with the MT9M001 camera module ***/
/* Enable DCMI clock */
RCC_AHB2PeriphClockCmd(RCC_AHB2Periph_DCMI, ENABLE);
/* DCMI configuration */
DCMI_InitStructure.DCMI_CaptureMode = DCMI_CaptureMode_Continuous;
DCMI_InitStructure.DCMI_SynchroMode = DCMI_SynchroMode_Hardware;
DCMI_InitStructure.DCMI_PCKPolarity = DCMI_PCKPolarity_Falling;
DCMI_InitStructure.DCMI_VSPolarity = DCMI_VSPolarity_High;
DCMI_InitStructure.DCMI_HSPolarity = DCMI_HSPolarity_High;
DCMI_InitStructure.DCMI_CaptureRate = DCMI_CaptureRate_All_Frame;
DCMI_InitStructure.DCMI_ExtendedDataMode = DCMI_ExtendedDataMode_10b;
/* Configures the DMA2 to transfer Data from DCMI */
/* Enable DMA2 clock */
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_DMA2, ENABLE);
/* DMA2 Stream1 Configuration */
DMA_DeInit(DMA2_Stream1);
DMA_InitStructure.DMA_Channel = DMA_Channel_1;
DMA_InitStructure.DMA_PeripheralBaseAddr = DCMI_DR_ADDRESS;
DMA_InitStructure.DMA_Memory0BaseAddr = FMC_SRAM_ADDRESS;
DMA_InitStructure.DMA_DIR = DMA_DIR_PeripheralToMemory;
DMA_InitStructure.DMA_BufferSize = 1;
DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable;
DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Enable;
DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_Word;
DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_HalfWord;
DMA_InitStructure.DMA_Mode = DMA_Mode_Circular;
DMA_InitStructure.DMA_Priority = DMA_Priority_High;
DMA_InitStructure.DMA_FIFOMode = DMA_FIFOMode_Enable;
DMA_InitStructure.DMA_FIFOThreshold = DMA_FIFOThreshold_Full;
DMA_InitStructure.DMA_MemoryBurst = DMA_MemoryBurst_Single;
DMA_InitStructure.DMA_PeripheralBurst = DMA_PeripheralBurst_Single;
DCMI_Init(&DCMI_InitStructure);
/* DMA2 IRQ channel Configuration */
DMA_Init(DMA2_Stream1, &DMA_InitStructure);
DMA_Cmd(DMA2_Stream1,ENABLE);
DCMI_Cmd(ENABLE);
}
Any help would be very usefull, since at this point, i don't know whats wrong