Skip to main content
Associate II
Apr 1, 2025 8:11 PM UTC
Solved

DBANK Option Byte default STM32G4

What is the default value of the DBANK bit in STM32G4 MCUs. According to the reference manual, flash memory address 0x1FFF 7800 has that option bit, and the ST production value is 0xFFEF F8AA, which would make DBANK default to 1. Does this mean STM32G4 MCUs have DBANK flash enabled by default, and do I need to do anything further to set it to DBANK? Or will it always be enabled out of the factory?

This topic has been closed for replies.
Igor Cesko
Igor CeskoBest answer
ST Employee
Apr 2, 2025 7:53 AM UTC

Dear tomm5771,

 

  Yes - Dual bank is enabled as default option for factory produced devices. There is no need to perform programming to have dual bank option on factory produced devices.

Regards

                      Igor

2 replies

Igor Cesko
Igor CeskoBest answer
ST Employee
Apr 2, 2025 7:53 AM UTC

Dear tomm5771,

 

  Yes - Dual bank is enabled as default option for factory produced devices. There is no need to perform programming to have dual bank option on factory produced devices.

Regards

                      Igor

tomm5771Author
Associate II
Apr 2, 2025 12:49 PM UTC

Thank you Igor. Much appreciated.