Question
Data transfer between two STM32 devices using FSMC
Posted on January 26, 2013 at 22:45
Hi,
I'm currious if it is possible to share data between two STM32 devices, using the FSMC interface. Is it possible to configure one device as a Master and the other as a slave and use the FSMC? I would make the slave device act, as it was a SRAM memory, for example. If not, is there a parallel peripheral to transfer data between two STM32 devices? Thanks in advance, Regards, A. Paiva