Skip to main content
Myasu.1
Associate III
February 20, 2024
Solved

Data is not stored in the FIFO when FSEL is 1

What I want to do is send Write Enable instruction to external Flash and erase.
The environment is as follows.

Use Board : nucleo l4r5zi
IDE : Atollic TrueSTUDIO® for STM32, Built on Eclipse Neon.1a.(Version: 9.3.0)
FLASH : W25Q64JV

The connection diagram of the board and FLASH is shown below.

Myasu1_0-1708448593094.png

I want to send Write Enable instruction to 「W25Q64JV 2」.
The registers are set as follows.

●OCTOSPI

Myasu1_1-1708448757561.png

●OCTOSPIM

Myasu1_2-1708449526837.png

I send Write Enable instruction and then the Read Status instruction. 0 is always stored in the FIFO. (Of course I make sure the FTF is set before reading the data register)

I assume that the setting on the microcontroller side is wrong because when I check IO5 with an oscilloscope, I get the expected waveform.

For your information, when I set FSEL to 0 and communicated with 「W25Q64JV 1」 using IO0~IO3, the data was stored in the FIFO as expected.

If there are any settings that are missing, I would like to know.

This topic has been closed for replies.
Myasu.1
Myasu.1Best answer
Associate III
February 23, 2024

Hello,

I changed the IO5 pin from PC2 to PG11 and now the data is stored in the FIFO as expected.

The problem has been solved and is closed.

1 reply

Myasu.1
Myasu.1AuthorBest answer
Associate III
February 23, 2024

Hello,

I changed the IO5 pin from PC2 to PG11 and now the data is stored in the FIFO as expected.

The problem has been solved and is closed.