Skip to main content
hospodar
Associate III
April 11, 2013
Question

Data from ADC to USART

  • April 11, 2013
  • 4 replies
  • 871 views
Posted on April 11, 2013 at 23:06

Hello, what changes must be performed in following code in order to send acquired data from ADC to USART and not to LCD (as it is now)?

/**
******************************************************************************
* @file ADC/Basic_example/main.c 
* @author MCD Application Team
* @version V1.0.0
* @date 18-May-2012
* @brief Main program body
******************************************************************************
* @attention
*
* <h2><center>© COPYRIGHT 2012 STMicroelectronics</center></h2>
*
* Licensed under MCD-ST Liberty SW License Agreement V2, (the ''License'');
* You may not use this file except in compliance with the License.
* You may obtain a copy of the License at:
*
* http://www.st.com/software_license_agreement_liberty_v2
*
* Unless required by applicable law or agreed to in writing, software 
* distributed under the License is distributed on an ''AS IS'' BASIS, 
* WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
* See the License for the specific language governing permissions and
* limitations under the License.
*
******************************************************************************
*/
/* Includes ------------------------------------------------------------------*/
#include ''main.h''
/** @addtogroup STM32F0xx_StdPeriph_Examples
* @{
*/
/** @addtogroup Basic_example
* @{
*/
/* Private typedef -----------------------------------------------------------*/
/* Private define ------------------------------------------------------------*/
#define MESSAGE1 ''STM32F05x CortexM0 '' 
#define MESSAGE2 '' STM320518-EVAL '' 
/* Private macro -------------------------------------------------------------*/
/* Private variables ---------------------------------------------------------*/
__IO uint16_t ADC1ConvertedValue = 0, ADC1ConvertedVoltage = 0;
ADC_InitTypeDef ADC_InitStructure;
GPIO_InitTypeDef GPIO_InitStructure;
/* Private function prototypes -----------------------------------------------*/
/* Private functions ---------------------------------------------------------*/
/**
* @brief Main program.
* @param None
* @retval None
*/
int
main(
void
)
{
/*!< At this stage the microcontroller clock setting is already configured, 
this is done through SystemInit() function which is called from startup
file (startup_stm32f0xx.s) before to branch to application main.
To reconfigure the default setting of SystemInit() function, refer to
system_stm32f0xx.c file
*/
/* LCD Display init */
Display_Init();
/* GPIOC Periph clock enable */
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOC, ENABLE);
/* ADC1 Periph clock enable */
RCC_APB2PeriphClockCmd(RCC_APB2Periph_ADC1, ENABLE);
/* Configure ADC Channel11 as analog input */
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_1 ;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AN;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL ;
GPIO_Init(GPIOC, &GPIO_InitStructure);
/* ADCs DeInit */
ADC_DeInit(ADC1);
/* Initialize ADC structure */
ADC_StructInit(&ADC_InitStructure);
/* Configure the ADC1 in continous mode withe a resolutuion equal to 12 bits */
ADC_InitStructure.ADC_Resolution = ADC_Resolution_12b;
ADC_InitStructure.ADC_ContinuousConvMode = ENABLE; 
ADC_InitStructure.ADC_ExternalTrigConvEdge = ADC_ExternalTrigConvEdge_None;
ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right;
ADC_InitStructure.ADC_ScanDirection = ADC_ScanDirection_Upward;
ADC_Init(ADC1, &ADC_InitStructure); 
/* Convert the ADC1 Channel 11 with 5 Cycles as sampling time */
ADC_ChannelConfig(ADC1, ADC_Channel_11 , ADC_SampleTime_239_5Cycles); 
/* ADC Calibration */
ADC_GetCalibrationFactor(ADC1);
/* Enable ADCperipheral[PerIdx] */
ADC_Cmd(ADC1, ENABLE); 
/* Wait the ADCEN falg */
while
(!ADC_GetFlagStatus(ADC1, ADC_FLAG_ADEN)); 
/* ADC1 regular Software Start Conv */
ADC_StartOfConversion(ADC1);
/* Infinite loop */
while
(1)
{
/* Test EOC flag */
while
(ADC_GetFlagStatus(ADC1, ADC_FLAG_EOC) == RESET);
/* Get ADC1 converted data */
ADC1ConvertedValue =ADC_GetConversionValue(ADC1);
/* Compute the voltage */
ADC1ConvertedVoltage = (ADC1ConvertedValue *3300)/0xFFF;
/* Display converted data on the LCD */
Display();
}
}
/**
* @brief Display ADC converted value on LCD
* @param None
* @retval None
*/
void
Display(
void
)
{
uint32_t v=0,mv=0;
uint8_t text[50];
v=(ADC1ConvertedVoltage)/1000;
mv = (ADC1ConvertedVoltage%1000)/100;
sprintf
((
char
*)text,
'' ADC = %d,%d V ''
,v,mv);
/* Set the LCD Back Color and Text Color*/
LCD_SetBackColor(White);
LCD_SetTextColor(Blue);
LCD_DisplayStringLine(LINE(6),text);
}
/**
* @brief Display Init (LCD)
* @param None
* @retval None
*/
void
Display_Init(
void
)
{
/* Initialize the LCD */
STM320518_LCD_Init();
/* Clear the LCD */
LCD_Clear(White);
/* Set the LCD Text size */
LCD_SetFont(&Font8x12);
/* Set the LCD Back Color and Text Color*/
LCD_SetBackColor(Blue);
LCD_SetTextColor(White);
/* Display */
LCD_DisplayStringLine(LINE(0x13), 
'' ADC conversion example (Basic example)''
);
/* Set the LCD Text size */
LCD_SetFont(&Font16x24);
LCD_DisplayStringLine(LINE(0), 
''STM32F05x CortexM0 ''
);
LCD_DisplayStringLine(LINE(1), 
'' STM320518-EVAL ''
);
/* Set the LCD Back Color and Text Color*/
LCD_SetBackColor(White);
LCD_SetTextColor(Blue);
/* Display */
LCD_DisplayStringLine(LINE(3),
'' Turn RV3(PC.01) ''
);
LCD_DisplayStringLine(LINE(4),
'' Potentiometer ''
);
}
/************************ (C) COPYRIGHT STMicroelectronics *****END OF FILE****/

    This topic has been closed for replies.

    4 replies

    Tesla DeLorean
    Guru
    April 11, 2013
    Posted on April 11, 2013 at 23:16

    In Keil, I'd retarget STDIO to use the USART and use printf().

    Alternatively you just initialize the USART and pins, and write a string output function.

    void USART_OutString(char *s)
    {
    while(*s)
    {
    while(USART_GetFlagStatus(USART1, USART_FLAG_TXE) == RESET); // Wait for Empty
    USART_SendData(USART1, *s++);
    }
    }

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Tesla DeLorean
    Guru
    April 11, 2013
    Posted on April 11, 2013 at 23:20

    Portable to STM32F2, adjust USART and pins as required.

    // STM32 USART1 (Tx PA.9, Rx PA.10) STM32F4 Discovery - sourcer32@gmail.com
    #include ''stm32f4_discovery.h''
    /**************************************************************************************/
    void RCC_Configuration(void)
    {
    /* --------------------------- System Clocks Configuration -----------------*/
    /* USART1 clock enable */
    RCC_APB2PeriphClockCmd(RCC_APB2Periph_USART1, ENABLE);
    /* GPIOA clock enable */
    RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA, ENABLE);
    }
    /**************************************************************************************/
    void GPIO_Configuration(void)
    {
    GPIO_InitTypeDef GPIO_InitStructure;
    /*-------------------------- GPIO Configuration ----------------------------*/
    GPIO_InitStructure.GPIO_Pin = GPIO_Pin_9 | GPIO_Pin_10;
    GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
    GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
    GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
    GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
    GPIO_Init(GPIOA, &GPIO_InitStructure);
    /* Connect USART pins to AF */
    GPIO_PinAFConfig(GPIOA, GPIO_PinSource9, GPIO_AF_USART1); // USART1_TX
    GPIO_PinAFConfig(GPIOA, GPIO_PinSource10, GPIO_AF_USART1); // USART1_RX
    }
    /**************************************************************************************/
    void USART1_Configuration(void)
    {
    USART_InitTypeDef USART_InitStructure;
    /* USARTx configuration ------------------------------------------------------*/
    /* USARTx configured as follow:
    - BaudRate = 9600 baud
    - Word Length = 8 Bits
    - One Stop Bit
    - No parity
    - Hardware flow control disabled (RTS and CTS signals)
    - Receive and transmit enabled
    */
    USART_InitStructure.USART_BaudRate = 9600;
    USART_InitStructure.USART_WordLength = USART_WordLength_8b;
    USART_InitStructure.USART_StopBits = USART_StopBits_1;
    USART_InitStructure.USART_Parity = USART_Parity_No;
    USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None;
    USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx;
    USART_Init(USART1, &USART_InitStructure);
    USART_Cmd(USART1, ENABLE);
    }
    /**************************************************************************************/
    void USART1_OutString(char *s)
    {
    while(*s)
    {
    while(USART_GetFlagStatus(USART1, USART_FLAG_TXE) == RESET); // Wait for Empty
    USART_SendData(USART1, *s++);
    }
    }
    /**************************************************************************************/
    int main(void)
    {
    RCC_Configuration();
    GPIO_Configuration();
    USART1_Configuration();
    while(1)
    {
    USART1_OutString(''Welcome to wherever you are!
    
    '');
    }
    while(1); // Don't want to exit
    }

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    hospodar
    hospodarAuthor
    Associate III
    April 12, 2013
    Posted on April 12, 2013 at 02:42

    I modified the code as follows. I added USART initialization and configuration, removed all command with LCD. I used printf in function ''

    Display()''

    ,

    which is retargered to the USART by the second code. However, it don´t working, I don´t receiving any data on the terminal. What is wrong?

    #include ''main.h''
    /** @addtogroup STM32F0xx_StdPeriph_Examples
    * @{
    */
    /** @addtogroup Basic_example
    * @{
    */
    /* Private typedef -----------------------------------------------------------*/
    /* Private define ------------------------------------------------------------*/
    #define MESSAGE1 ''STM32F05x CortexM0 ''
    #define MESSAGE2 '' STM320518-EVAL ''
    /* Private macro -------------------------------------------------------------*/
    /* Private variables ---------------------------------------------------------*/
    __IO uint16_t ADC1ConvertedValue = 0, ADC1ConvertedVoltage = 0;
    ADC_InitTypeDef ADC_InitStructure;
    GPIO_InitTypeDef GPIO_InitStructure;
    USART_InitTypeDef USART_InitStructure;
    /* Private function prototypes -----------------------------------------------*/
    /* Private functions ---------------------------------------------------------*/
    /**
    * @brief Main program.
    * @param None
    * @retval None
    */
    int

    main(

    void

    )
    {
    /*!< At this stage the microcontroller clock setting is already configured,
    this is done through SystemInit() function which is called from startup
    file (startup_stm32f0xx.s) before to branch to application main.
    To reconfigure the default setting of SystemInit() function, refer to
    system_stm32f0xx.c file
    */
    /* GPIOC and A Periph clock enable */
    RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOC, ENABLE);
    RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA, ENABLE);
    /* ADC1 Periph clock enable */
    RCC_APB2PeriphClockCmd(RCC_APB2Periph_ADC1, ENABLE);
    /* Povolenie hodin pre USART */
    RCC_APB2PeriphClockCmd(RCC_APB2Periph_USART1, ENABLE);
    /* Premapovanie pinov PA9 a PA10 na USART */
    GPIO_PinAFConfig(GPIOA,GPIO_PinSource9,GPIO_AF_1);
    GPIO_PinAFConfig(GPIOA,GPIO_PinSource10,GPIO_AF_1);
    /* USART TX ako alternativna funkcia */
    GPIO_InitStructure.GPIO_Pin = GPIO_Pin_9;
    GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
    GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
    GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
    GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
    GPIO_Init(GPIOA, &GPIO_InitStructure);
    /* Nastavenie USART Rx pre prijem */
    GPIO_InitStructure.GPIO_Pin = GPIO_Pin_10;
    GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN;
    GPIO_Init(GPIOA, &GPIO_InitStructure);
    /* Nastavenie parametrov seriovej linky USART
    pomocou inicializacnej struktury */
    USART_InitStructure.USART_BaudRate = 115200;
    // Bitova rychlost - 115200 baud
    USART_InitStructure.USART_WordLength = USART_WordLength_8b;
    // Dlzka slova - 8 bit
    USART_InitStructure.USART_StopBits = USART_StopBits_1;
    // Jeden stop-bit
    USART_InitStructure.USART_Parity = USART_Parity_No;
    // Bez parity
    USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None;
    // Hardverove riadenie (RTS,CTS) vypnute
    USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx;
    // Prijimanie a vysielanie povolene
    USART_Init(USART1, &USART_InitStructure);
    // Inicializacia USART zo struktury
    /* Configure ADC Channel11 as analog input */
    GPIO_InitStructure.GPIO_Pin = GPIO_Pin_1 ;
    GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AN;
    GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL ;
    GPIO_Init(GPIOC, &GPIO_InitStructure);
    /* ADCs DeInit */
    ADC_DeInit(ADC1);
    /* Initialize ADC structure */
    ADC_StructInit(&ADC_InitStructure);
    /* Configure the ADC1 in continous mode withe a resolutuion equal to 12 bits */
    ADC_InitStructure.ADC_Resolution = ADC_Resolution_12b;
    ADC_InitStructure.ADC_ContinuousConvMode = ENABLE;
    ADC_InitStructure.ADC_ExternalTrigConvEdge = ADC_ExternalTrigConvEdge_None;
    ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right;
    ADC_InitStructure.ADC_ScanDirection = ADC_ScanDirection_Upward;
    ADC_Init(ADC1, &ADC_InitStructure);
    /* Convert the ADC1 Channel 11 with 5 Cycles as sampling time */
    ADC_ChannelConfig(ADC1, ADC_Channel_11 , ADC_SampleTime_239_5Cycles);
    /* ADC Calibration */
    ADC_GetCalibrationFactor(ADC1);
    /* Enable ADCperipheral[PerIdx] */
    ADC_Cmd(ADC1, ENABLE);
    USART_Cmd(USART1, ENABLE);
    /* Wait the ADCEN falg */
    while

    (!ADC_GetFlagStatus(ADC1, ADC_FLAG_ADEN));
    /* ADC1 regular Software Start Conv */
    ADC_StartOfConversion(ADC1);
    /* Infinite loop */
    while

    (1)
    {
    /* Test EOC flag */
    while

    (ADC_GetFlagStatus(ADC1, ADC_FLAG_EOC) == RESET);
    /* Get ADC1 converted data */
    ADC1ConvertedValue =ADC_GetConversionValue(ADC1);
    /* Compute the voltage */
    ADC1ConvertedVoltage = (ADC1ConvertedValue *3300)/0xFFF;
    /* Display converted data on the LCD */
    Display();
    }
    }
    void

    Display(

    void

    )
    {
    uint32_t v=0,mv=0;
    uint8_t text[50];
    v=(ADC1ConvertedVoltage)/1000;
    mv = (ADC1ConvertedVoltage%1000)/100;
    printf

    ((

    char

    *)text,

    '' ADC = %d,%d V ''

    ,v,mv);
    }

    Hosting of stdio functionality through USART1:

    #include <rt_misc.h>
    #include ''stdio_through_usart.h''
    #include ''stm32f0xx.h''
    #include ''periph_init.h''
    #include <stdio.h>
    #pragma import(__use_no_semihosting_swi)
    struct

    __FILE {

    int

    handle;

    /* Add whatever you need here */

    };
    FILE

    __stdout;
    FILE

    __stdin;
    int
    fputc

    (

    int

    ch,

    FILE

    *f)
    {
    while

    (USART_GetFlagStatus(USART1, USART_FLAG_TXE) == RESET);
    USART_SendData(USART1, ch);
    return

    (ch);
    }
    int
    fgetc

    (

    FILE

    *f)
    {
    char

    ch;
    while

    (USART_GetFlagStatus(USART1, USART_FLAG_RXNE) == RESET);
    ch = USART_ReceiveData(USART1);
    return

    ((

    int

    )ch);
    }
    int
    ferror

    (

    FILE

    *f)
    {
    /* Your implementation of ferror */
    return

    EOF;
    }
    void

    _ttywrch(

    int

    ch)
    {
    while

    (USART_GetFlagStatus(USART1, USART_FLAG_TXE) == RESET);
    USART_SendData(USART1, ch);
    }
    void

    _sys_exit(

    int

    return_code)
    {
    label:

    goto

    label;

    /* endless loop */

    }
    //******************************************************************************

    Tesla DeLorean
    Guru
    April 12, 2013
    Posted on April 12, 2013 at 03:10

    Noticed it was an F0, sorry.

    void Display(void)
    {
    uint32_t v=0,mv=0;
    v=(ADC1ConvertedVoltage)/1000;
    mv = (ADC1ConvertedVoltage%1000)/100;
    printf('' ADC = %d,%d V 
    
    '',v,mv);
    }

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..