Skip to main content
TPanc.1
Associate II
August 9, 2021
Question

DAC with DMA not working for STM32H753VIT6

  • August 9, 2021
  • 10 replies
  • 4123 views

Hi there,

Here is the code for DAC with DMA. I can not see the error in the code. I have been looking at the oscilloscope for the sine wave but it is not coming. I tried without DMA, and works nice. But the DAC with DMA is not working. Please someone guide me. Thanks.

/* USER CODE BEGIN PV */

uint32_t sine_val[100];

/* USER CODE END PV */

/* USER CODE BEGIN PFP */

void get_sineval(void);

/* USER CODE END PFP */

int main(void)

{

 /* USER CODE BEGIN 1 */

 /* USER CODE END 1 */

 /* MCU Configuration--------------------------------------------------------*/

 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */

 HAL_Init();

 /* USER CODE BEGIN Init */

 /* USER CODE END Init */

 /* Configure the system clock */

 SystemClock_Config();

/* Configure the peripherals common clocks */

 PeriphCommonClock_Config();

 /* USER CODE BEGIN SysInit */

 /* USER CODE END SysInit */

 /* Initialize all configured peripherals */

 MX_GPIO_Init();

 MX_DMA_Init();

 MX_ADC1_Init();

 MX_ADC3_Init();

 MX_DAC1_Init();

 MX_I2C1_Init();

 MX_SPI1_Init();

 MX_SPI2_Init();

 MX_SPI3_Init();

 MX_SPI4_Init();

 MX_UART4_Init();

 MX_UART5_Init();

 MX_TIM1_Init();

 MX_TIM6_Init();

 /* USER CODE BEGIN 2 */

 if (HAL_TIM_Base_Start(&htim6) != HAL_OK)

 Error_Handler();

 get_sineval();

 if (HAL_DAC_Start_DMA(&hdac1, DAC_CHANNEL_2, (uint32_t *)sine_val, 100, DAC_ALIGN_12B_R) != HAL_OK)

 Error_Handler();

 /* USER CODE END 2 */

 /* Infinite loop */

 /* USER CODE BEGIN WHILE */

 while (1)

 {

  /* USER CODE END WHILE */

  /* USER CODE BEGIN 3 */

 }

 /* USER CODE END 3 */

}

void get_sineval()

{

for (int i=0;i<100;i++)

{

sine_val[i] = ((sin(i*2*pi/100)+1)*(4096/2));

}

}

Also, find the driver for DAC and Timer6 as below:

void MX_TIM6_Init(void)

{

 /* USER CODE BEGIN TIM6_Init 0 */

 /* USER CODE END TIM6_Init 0 */

 TIM_MasterConfigTypeDef sMasterConfig = {0};

 /* USER CODE BEGIN TIM6_Init 1 */

 /* USER CODE END TIM6_Init 1 */

 htim6.Instance = TIM6;

 htim6.Init.Prescaler = 96-1;

 htim6.Init.CounterMode = TIM_COUNTERMODE_UP;

 htim6.Init.Period = 100-1;

 htim6.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;

 if (HAL_TIM_Base_Init(&htim6) != HAL_OK)

 {

  Error_Handler();

 }

 sMasterConfig.MasterOutputTrigger = TIM_TRGO_UPDATE;

 sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;

 if (HAL_TIMEx_MasterConfigSynchronization(&htim6, &sMasterConfig) != HAL_OK)

 {

  Error_Handler();

 }

 /* USER CODE BEGIN TIM6_Init 2 */

 /* USER CODE END TIM6_Init 2 */

}

void MX_DAC1_Init(void)

{

 /* USER CODE BEGIN DAC1_Init 0 */

 /* USER CODE END DAC1_Init 0 */

 DAC_ChannelConfTypeDef sConfig = {0};

 /* USER CODE BEGIN DAC1_Init 1 */

 /* USER CODE END DAC1_Init 1 */

 /** DAC Initialization

 */

 hdac1.Instance = DAC1;

 if (HAL_DAC_Init(&hdac1) != HAL_OK)

 {

  Error_Handler();

 }

 /** DAC channel OUT2 config

 */

 sConfig.DAC_SampleAndHold = DAC_SAMPLEANDHOLD_DISABLE;

 sConfig.DAC_Trigger = DAC_TRIGGER_T6_TRGO;

 sConfig.DAC_OutputBuffer = DAC_OUTPUTBUFFER_ENABLE;

 sConfig.DAC_ConnectOnChipPeripheral = DAC_CHIPCONNECT_DISABLE;

 sConfig.DAC_UserTrimming = DAC_TRIMMING_FACTORY;

 if (HAL_DAC_ConfigChannel(&hdac1, &sConfig, DAC_CHANNEL_2) != HAL_OK)

 {

  Error_Handler();

 }

 /* USER CODE BEGIN DAC1_Init 2 */

 /* USER CODE END DAC1_Init 2 */

}

This topic has been closed for replies.

10 replies

AbidSulaiman
Associate II
August 9, 2021

Hi,

is the DMA configured correctly, connected to the DAC?

I am not really familiar with DAC and your microcontroller, but from the MX_DAC1_Init(), I didn't see the DMA Enable bit being set.

Note: Please use the code snippet feature. It makes the reading easier (at least for me).

Regards

TPanc.1
TPanc.1Author
Associate II
August 9, 2021

Hi, I have tried initializing the void HAL_DAC_MspInit(DAC_HandleTypeDef* dacHandle) function within the MX_DAC1_init() function. But still does not work. Please let me know if you found some thing more.

DAC_HandleTypeDef hdac1;
DMA_HandleTypeDef hdma_dac1_ch2;
 
/* DAC1 init function */
void MX_DAC1_Init(void)
{
 
 /* USER CODE BEGIN DAC1_Init 0 */
 
 /* USER CODE END DAC1_Init 0 */
 
 DAC_ChannelConfTypeDef sConfig = {0};
 
 /* USER CODE BEGIN DAC1_Init 1 */
 
 /* USER CODE END DAC1_Init 1 */
 /** DAC Initialization
 */
 hdac1.Instance = DAC1;
 if (HAL_DAC_Init(&hdac1) != HAL_OK)
 {
 Error_Handler();
 }
 /** DAC channel OUT2 config
 */
 sConfig.DAC_SampleAndHold = DAC_SAMPLEANDHOLD_DISABLE;
 sConfig.DAC_Trigger = DAC_TRIGGER_T6_TRGO;
 sConfig.DAC_OutputBuffer = DAC_OUTPUTBUFFER_ENABLE;
 sConfig.DAC_ConnectOnChipPeripheral = DAC_CHIPCONNECT_DISABLE;
 sConfig.DAC_UserTrimming = DAC_TRIMMING_FACTORY;
 if (HAL_DAC_ConfigChannel(&hdac1, &sConfig, DAC_CHANNEL_2) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN DAC1_Init 2 */
 HAL_DAC_MspInit(&hdac1);
 /* USER CODE END DAC1_Init 2 */
 
}
 
void HAL_DAC_MspInit(DAC_HandleTypeDef* dacHandle)
{
 
 GPIO_InitTypeDef GPIO_InitStruct = {0};
 if(dacHandle->Instance==DAC1)
 {
 /* USER CODE BEGIN DAC1_MspInit 0 */
 
 /* USER CODE END DAC1_MspInit 0 */
 /* DAC1 clock enable */
 __HAL_RCC_DAC12_CLK_ENABLE();
 
 __HAL_RCC_GPIOA_CLK_ENABLE();
 /**DAC1 GPIO Configuration
 PA5 ------> DAC1_OUT2
 */
 GPIO_InitStruct.Pin = GPIO_PIN_5;
 GPIO_InitStruct.Mode = GPIO_MODE_ANALOG;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
 
 /* DAC1 DMA Init */
 /* DAC1_CH2 Init */
 hdma_dac1_ch2.Instance = DMA1_Stream0;
 hdma_dac1_ch2.Init.Request = DMA_REQUEST_DAC2;
 hdma_dac1_ch2.Init.Direction = DMA_MEMORY_TO_PERIPH;
 hdma_dac1_ch2.Init.PeriphInc = DMA_PINC_DISABLE;
 hdma_dac1_ch2.Init.MemInc = DMA_MINC_ENABLE;
 hdma_dac1_ch2.Init.PeriphDataAlignment = DMA_PDATAALIGN_WORD;
 hdma_dac1_ch2.Init.MemDataAlignment = DMA_MDATAALIGN_WORD;
 hdma_dac1_ch2.Init.Mode = DMA_CIRCULAR;
 hdma_dac1_ch2.Init.Priority = DMA_PRIORITY_LOW;
 hdma_dac1_ch2.Init.FIFOMode = DMA_FIFOMODE_DISABLE;
 if (HAL_DMA_Init(&hdma_dac1_ch2) != HAL_OK)
 {
 Error_Handler();
 }
 
 __HAL_LINKDMA(dacHandle,DMA_Handle2,hdma_dac1_ch2);
 
 /* DAC1 interrupt Init */
 HAL_NVIC_SetPriority(TIM6_DAC_IRQn, 0, 0);
 HAL_NVIC_EnableIRQ(TIM6_DAC_IRQn);
 /* USER CODE BEGIN DAC1_MspInit 1 */
 
 /* USER CODE END DAC1_MspInit 1 */
 }
}

AbidSulaiman
Associate II
August 9, 2021

Hi,

I think HAL_DAC_MspInit() is called within the HAL_DAC_Init() function.

I think I see nothing wrong with the code. So maybe check your hardware or circuit again.

Sorry that i could not help you further. Good luck.

Regards

MasterT
Lead II
August 9, 2021

DMA_REQUEST_DAC2 but initially you configured DAC1 ?

And where is config TIM6 ?

TPanc.1
TPanc.1Author
Associate II
August 9, 2021

Here is the initialization function for TIM6. Sorry that I am putting everything bit by bit. And, yes. I do not know why the CubeMX is generating DMA_REQUEST_DAC2. I updated it to DMA_REQUEST_DAC. But the status remains the same. No sine wave.

void MX_TIM6_Init(void)
{
 
 /* USER CODE BEGIN TIM6_Init 0 */
 
 /* USER CODE END TIM6_Init 0 */
 
 TIM_MasterConfigTypeDef sMasterConfig = {0};
 
 /* USER CODE BEGIN TIM6_Init 1 */
 
 /* USER CODE END TIM6_Init 1 */
 htim6.Instance = TIM6;
 htim6.Init.Prescaler = 96-1;
 htim6.Init.CounterMode = TIM_COUNTERMODE_UP;
 htim6.Init.Period = 100-1;
 htim6.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;
 if (HAL_TIM_Base_Init(&htim6) != HAL_OK)
 {
 Error_Handler();
 }
 sMasterConfig.MasterOutputTrigger = TIM_TRGO_UPDATE;
 sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
 if (HAL_TIMEx_MasterConfigSynchronization(&htim6, &sMasterConfig) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN TIM6_Init 2 */
 HAL_TIM_Base_MspInit(&htim6);
 /* USER CODE END TIM6_Init 2 */
 
}
 
void HAL_TIM_Base_MspInit(TIM_HandleTypeDef* tim_baseHandle)
{
 
 if(tim_baseHandle->Instance==TIM1)
 {
 /* USER CODE BEGIN TIM1_MspInit 0 */
 
 /* USER CODE END TIM1_MspInit 0 */
 /* TIM1 clock enable */
 __HAL_RCC_TIM1_CLK_ENABLE();
 /* USER CODE BEGIN TIM1_MspInit 1 */
 
 /* USER CODE END TIM1_MspInit 1 */
 }
 else if(tim_baseHandle->Instance==TIM6)
 {
 /* USER CODE BEGIN TIM6_MspInit 0 */
 
 /* USER CODE END TIM6_MspInit 0 */
 /* TIM6 clock enable */
 __HAL_RCC_TIM6_CLK_ENABLE();
 /* USER CODE BEGIN TIM6_MspInit 1 */
 
 /* USER CODE END TIM6_MspInit 1 */
 }
}

TDK
August 9, 2021
"If you feel a post has answered your question, please click ""Accept as Solution""."
TPanc.1
TPanc.1Author
Associate II
August 9, 2021

I did something like this to clean the cache. But no change. The DMA and DAC both are in D2 region. I am not sure whether to move further in this direction.

 /* USER CODE BEGIN 2 */
 /* Clean D-cache */
 /* Make sure the address is 32-byte aligned and add 32-bytes to length, in case it overlaps cacheline */
 SCB_CleanDCache_by_Addr((uint32_t*)(((uint32_t)sine_val) & ~(uint32_t)0x1F), 100);
// HAL_DAC_Start(&hdac1, DAC_CHANNEL_2);	//un-comment incase of polling technique/without DMA
 get_sineval();
 if (HAL_TIM_Base_Start(&htim6) != HAL_OK)
	 Error_Handler();
 
__DSB(); 
 if (HAL_DAC_Start_DMA(&hdac1, DAC_CHANNEL_2, (uint32_t *)sine_val, 100, DAC_ALIGN_12B_R) != HAL_OK)
	 Error_Handler();
 
 /* USER CODE END 2 */

TDK
August 9, 2021
"If you feel a post has answered your question, please click ""Accept as Solution""."