Skip to main content
gurnett2
Associate II
March 9, 2012
Question

CUSTOMHID_SIZ_REPORT_DESC larger than 255

  • March 9, 2012
  • 3 replies
  • 1061 views
Posted on March 09, 2012 at 12:29

I have a hid report created using descriptor tool 2.4. The final descriptor size is 289. which appears to be to large (hid not detected). If I cut a few reports out so the size becomes less than 256 it works fine. Is it possible to increase the limit or do I need to do something else to get around this.

I'm using STM32_USB-FS-Device_Lib_V3.3.0

Thank you

Michael
    This topic has been closed for replies.

    3 replies

    tsuneo
    Associate II
    March 10, 2012
    Posted on March 10, 2012 at 02:27

    Fix wItemLength field of HID descriptor (in the config descriptor set), as follows

    usb_desc.c

    #define WBVAL(x) (x & 0xFF),((x >> 8) & 0xFF)    // <--- add this definition

    const uint8_t CustomHID_ConfigDescriptor[CUSTOMHID_SIZ_CONFIG_DESC] =

      {

        ...

        ...

        /******************** Descriptor of Custom HID HID ********************/

        /* 18 */

        0x09,         /* bLength: HID Descriptor size */

        HID_DESCRIPTOR_TYPE, /* bDescriptorType: HID */

        0x10,         /* bcdHID: HID Class Spec release number */

        0x01,

        0x00,         /* bCountryCode: Hardware target country */

        0x01,         /* bNumDescriptors: Number of HID class descriptors to follow */

        0x22,         /* bDescriptorType */

                                               // modify these two lines

    //    CUSTOMHID_SIZ_REPORT_DESC,/* wItemLength: Total length of Report descriptor */

    //    0x00,

        WBVAL( CUSTOMHID_SIZ_REPORT_DESC ), /* wItemLength: Total length of Report descriptor */

    Tsuneo

    gurnett2
    gurnett2Author
    Associate II
    March 10, 2012
    Posted on March 10, 2012 at 18:19

    Thanks

    I figured it out an your suggestion is pretty much what I did which confirms that I was on the right track

    -Michael

    tsuneo
    Associate II
    March 10, 2012
    Posted on March 10, 2012 at 18:58

    > your suggestion is pretty

    Thanks,

    but such a macro is a standard way to fill two-bytes numbers into descriptors.

    You'll see this way in many USB examples from other resources.

    If ST team would learn the standard way, you shouldn't be trapped.

    Tsuneo