Solved
GyessineBest answer
ST Technical Moderator
February 25, 2026
Hello
There are several actions that you can take to troubleshoot the root cause of the issue.
First, test your project on a reference board as suggested by
It is also advisable to isolate the USB component from TouchGFX when testing on both boards to determine whether the problem is due to a hardware implementation or a software issue.
If the USB functions correctly in isolation, test the entire project on both boards.Maybe TouchGFX is interfering with USB functionality.
BR
Gyessine
In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.