Skip to main content
Associate
August 4, 2023
Question

Custom PCB detection

I designed a PCB using STM32L476RG and MPU6050. I used USB interface in the board. When I am connecting the board to my laptop the board is getting the power but laptop is unable to detect the board. Should I install any drivers in my laptop to make that work or is there anything else. Please help me with this. 

This topic has been closed for replies.

8 replies

TDK
August 4, 2023

You need code on the processor which initializes USB and handles communication. Did you do that?

Dev boards have an ST-Link between the target MCU and the PC used for programming and communication. If you connect an MCU directly, this interface is not there.

"If you feel a post has answered your question, please click ""Accept as Solution""."
Associate
August 4, 2023

Thank you for the response I did program the PCB using STLINK - V3MINIE. I can see in the console of STM32CubeIDE the target device name and it says download is successful when running the code. But I cannot see it in the COM port section of device manager. What might be the possible reason for this, How do I rectify that?

Tesla DeLorean
Guru
August 4, 2023

Is the code you're uploading a USB CDC Device?

If it's not working, expect to have to debug it.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
waclawek.jan
Super User
August 4, 2023

> You need code on the processor which initializes USB and handles communication.

Some of the STM32 have built-in USB-DFU bootloader. Refer to AN2606 and any other document linked from there.

JW

Tesla DeLorean
Guru
August 4, 2023

Would appear as an "STM32 BOOT" device in DFU mode if reset with BOOT0 pulled HIGH, this would allow programming via STM32 Cube Programmer.

A device with no code running on it won't be any type of USB Device. You'd need a application loaded and running.

STM32Cube_FW_L4_V1.17.2\Projects\32L476GDISCOVERY\Applications\USB_Device\DFU_Standalone

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
waclawek.jan
Super User
August 5, 2023

> But I cannot see it in the COM port section of device manager.

Do you see it elsewhere?

After programming with code, did you change the BOOT0 pin setting (or any other setting to avoid repeated bootloader entry) and did you remove and reconnect power?

JW