Skip to main content
MBish.1
Associate II
May 23, 2023
Solved

Currently we make use of three SPI busses on a STM32F405. SPI1 is a slave and SPI 2/3 are masters. I switch SPI1 to master mode and it just doesn't work. I suspect the APB2 bus but I think I have it set correctly.

Here's my code:

SPI_HandleTypeDef spi_handle =
 {
 .Instance = DEF_SPI_INS_SPI1,
 .Init =
 {
 .Direction = SPI_DIRECTION_2LINES,
 .BaudRatePrescaler = SPI_BAUDRATEPRESCALER_2, 
 .CLKPhase = SPI_PHASE_2EDGE, 
 .CLKPolarity = SPI_POLARITY_HIGH, 
 .CRCCalculation = SPI_CRCCALCULATION_DISABLE,
 .CRCPolynomial = 0U, // unused
 .DataSize = SPI_DATASIZE_8BIT,
 .FirstBit = SPI_FIRSTBIT_MSB,
 .NSS = SPI_NSS_SOFT,
 .TIMode = SPI_TIMODE_DISABLE,
 .Mode = SPI_MODE_MASTER
 }
 };
 
 HAL_StatusTypeDef return_code;
 return_code = HAL_SPI_Init(&spi_handle);
 uint8_t data[] = {0x01, 0x02, 0x03, 0x04, 0x05, 0x06, 0x07, 0x08};
 uint8_t rx_data[16];
 
 HAL_SPI_Abort(&spi_handle);
 __HAL_SPI_ENABLE(&spi_handle);
 //return_code = HAL_SPI_Transmit(&spi_handle, data, 8, 5);
 return_code = HAL_SPI_TransmitReceive(&spi_handle, data, rx_data, 8, 100);
 
 while (HAL_SPI_GetState(&spi_handle) != HAL_SPI_STATE_READY);

return_code from HAL_SPI_Init() == HAL_OK

return code from HAL_SPI_TransmitReceive() == HAL_OK

I get past the while{} loop.

SPI register settings:


_legacyfs_online_stmicro_images_0693W00000bklpzQAA.pngPIOA settings (pins 5 = SCLK, 6 = MOSI, 7 = MISO):


_legacyfs_online_stmicro_images_0693W00000bkhu2QAA.png
_legacyfs_online_stmicro_images_0693W00000bkhuqQAA.png
_legacyfs_online_stmicro_images_0693W00000bkhugQAA.png
_legacyfs_online_stmicro_images_0693W00000bkhuCQAQ.pngRCC register settings:


_legacyfs_online_stmicro_images_0693W00000bkhv5QAA.png
_legacyfs_online_stmicro_images_0693W00000bkhvPQAQ.png 

I've played around with the prescaler CLK phase and polarity. One note, CLK never idles HIGH with CPOL = SPI_POLARITY_HIGH.

What am I missing?

This is all I get when I am in master mode:

Also note, I am not wiggling a CS right now - just trying to see a CLK and some data.


_legacyfs_online_stmicro_images_0693W00000bkhwcQAA.pngWhen I build it in slave mode and send data to the chip I see nice wiggles in all the right places and the micro reads the data correctly and sends back data to the remote SPI master. When I am doing this mcu SPI master testing, I have the remote master device disconnected and just have the logic analyzer connected.

This topic has been closed for replies.
MBish.1
MBish.1Best answer
Associate II
May 24, 2023

This was a hardware issue.

6 replies

waclawek.jan
Super User
May 24, 2023

Are you sure you want SPI_CR1.BIDIMODE be set?

JW

MBish.1
MBish.1Author
Associate II
May 24, 2023

I tried it again with that cleared, updated the image and still the same results.

waclawek.jan
Super User
May 24, 2023

OK so set SCK to GPIO Output and try to wiggle it "manually" and observe.

JW

MBish.1
MBish.1Author
Associate II
May 24, 2023

I can't wiggle the old CLK and SDI. I can wiggle SDO.

Bob S
Super User
May 24, 2023

What external device is connected to the SPI signals? Is whatever used to be the master still connected? If so, it is probably driving those signals.

MBish.1
MBish.1AuthorBest answer
Associate II
May 24, 2023

This was a hardware issue.