Skip to main content
Code Wrangler
Associate II
September 27, 2017
Question

CubeMX Wish List

  • September 27, 2017
  • 3 replies
  • 1036 views

Posted on September 27, 2017 at 23:05

I wanted to submit some suggested improvements to the '

<LINK NO LONGER ACTIVE>

' discussion, but unfortunately that thread is closed and locked. Since these suggestions don't do any good sitting in a text file on my computer, I wanted to create a new thread to record these. They are listed in terms of priority / usefulness to me:

1. Display calculated ADC & timer frequencies (and periods [in time units] and duty cycles [in percent]) the way it is currently done for SPI

2. Be able to make labels for interrupts in the NVIC interrupt table. Also the label should get a descriptive default name (i.e. 'SPI1 DMA Interrupt' instead of the current 'DMA1 Stream6 Interrupt')

3. Be able to setup GPIO DMA transfers, with optional timer triggers

4. Be able to create memory-to-memory transfers with timer triggers

    This topic has been closed for replies.

    3 replies

    john doe
    Senior III
    September 27, 2017
    Posted on September 28, 2017 at 01:49

    1. have a feature freeze and spend a couple release cycles just getting the existing code right

    2. actually test the code that the cubemx application generates.  generate the code for 'blink' and upload it to a supported board and see if it actually works.

    Nesrine M_O
    Associate
    September 28, 2017
    Posted on September 28, 2017 at 11:39

    Hi

    homert2014

    ,

    Thanks for the suggestion! I will forward this to our MX team.

    If we have other suggestionsabout HAL,please submit it inother thread.

    -Nesrine

    Code Wrangler
    Associate II
    September 28, 2017
    Posted on September 28, 2017 at 14:38

    Ok, I have changed it to only a CubeMX wish list.

    I haven't found any HAL bugs so far. If I find one, I will start a HAL thread.