Question
CubeMX USART LL Configuration not Working!
Posted on June 04, 2018 at 09:54
Dear friends,
I am trying to send 8 bytes over RS485 protocol using LL libraries.
I could achieve sending data using HAL libraries (CubeMX configuration) and
SPL libraries.
Now I want to use LL APIs to transmit data. I've used the following code:
DE_SIGNAL_GPIO_Port->BSRR = DE_SIGNAL_Pin;
LL_mDelay(100); for(j=0;j<8;j++) { while(!LL_USART_IsActiveFlag_TXE(USART1)){} LL_USART_TransmitData8(USART1,snd_buff[j]); } while(!LL_USART_IsActiveFlag_TC(USART1)){} DE_SIGNAL_GPIO_Port->BRR = DE_SIGNAL_Pin;The code is not working and no data is transmitted.
The SPL counterpart code that works fine is as follow:
GPIOA->BSRR=GPIO_Pin_8;for(i=0;i<Length+2;i++)
{ while(USART_GetFlagStatus(USART1,USART_FLAG_TXE)==RESET){} USART1->DR = snd_buff[i]; } while(USART_GetFlagStatus(USART1,USART_FLAG_TC)==RESET){}GPIOA->BRR=GPIO_Pin_8;
I'll be thankful if anyone could help run the USART using LL APIs.