Posted on December 16, 2016 at 12:37 Dear
Downey.Elwood
,
After checking, this is not a bug, as
clock for
I2S1 mapped on APB2 and clock for I2S2 mapped on APB1.
This is mentioned in the RM0390 (page 116):
'
I2S1/2 clocks
To achieve high-quality audio performance and for a better configuration flexibility, the I2S1 clock and I2S2 clock (which are respectively clocks for I2Ss mapped on APB1 and APB2) can be derived from four sources: specific main PLL output, a specific PLLI2S output, from an external clock mapped on the I2S_CKIN pin or from HSI/HSE
'
Best Regards
-Imen-
In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks