Skip to main content
smhhadima
Associate III
May 23, 2016
Question

CubeMX: SD_Card SPI

  • May 23, 2016
  • 0 replies
  • 447 views
Posted on May 23, 2016 at 08:35

How can I use the SPI to write to SD_Card (with HAL lib.) 

because CubeMx forces me to use SDIO which I have no access to it.

is there is an HAL example using SPI to drive the SD card?
    This topic has been closed for replies.