Skip to main content
David Fisher
Associate II
Jan 9, 2018 6:15 PM UTC
Question

CubeMX project settings dialog in ubuntu, hitting enter key doesn't click buttons, but does in windows ?

Posted on January 09, 2018 at 19:15

I am trying to use CubeMX on ubuntu but as explained in previous posts I can't see the ok and cancel buttons in the project settings dialog, so I can't click them with the mouse.  In windows  I can tab to the buttons and then hitting enter activates their command. In ubuntu tabbing to the hidden buttons and hitting enter doesn't work, not even for the visible browse button for the project location. How do I activate the buttons in the project settings dialog in ubuntu with the keyboard ?

edit: I have just found that by setting my screen settings to scale 100% I can see the buttons. Though everything is very tiny on my 32' screen. But the question still stands why can't I use the enter key to activate the buttons ?

Regards

    This topic has been closed for replies.

    2 replies

    Andrew Neil
    Super User
    Jan 9, 2018 6:19 PM UTC
    Posted on January 09, 2018 at 19:19

    as explained in previous posts

    links would be helpful ...

    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
    David Fisher
    Associate II
    Jan 9, 2018 8:02 PM UTC
    Posted on January 09, 2018 at 20:02

    Iwas thinking people would click on my name and get the links from there. I hate it too when people don't just link.

    As in the edit I can now generate code on ubuntu but why can't I hit enter to click the buttons ?

    https://community.st.com/0D50X00009XkYA2SAN

    https://community.st.com/0D50X00009XkYA0SAN