Skip to main content
Sidlauskas.David
Associate III
March 16, 2018
Question

CubeMx Generates Garbage Init Code??

  • March 16, 2018
  • 3 replies
  • 966 views
Posted on March 16, 2018 at 02:05

Using CubeMX V4.7.1 I get garbage initialization code for RTC.c when I request initialization be generated as .c.h file pairs.

Simple demo case:

Start CubeMX

New Project

Select STMf103C8Tx as target

Under Pins Select RTC-> Activate Clock Source.

Under Project settings:

   Project Name: Test

   Location: C:\Temp\

   Under Code Generator Tab:

         Check Generate peripheral initialization as pair of .c/.h files

Leave everything else at defaults.

Generate the code and look at rtc.c. It's not C source code. Eg.

/* RTC init function */

void MX_RTC_Init(void)

{

#n

#t#t/**Initialize RTC Only #n#t#t*/

#thrtc.Instance = RTC;

#thrtc.Init.AsynchPrediv = RTC_AUTO_1_SECOND;

#thrtc.Init.OutPut = RTC_OUTPUTSOURCE_ALARM;

#tif (HAL_RTC_Init(&hrtc) != HAL_OK)

#t{

#t#t_Error_Handler(__FILE__, __LINE__);

#t}

Followed by what looks like a lot of Java error messages.

Looks like a CubeMX bug to me. If I leave the init stuff in main, it works OK.

Dave

This topic has been closed for replies.

3 replies

ST Technical Moderator
March 16, 2018
Posted on March 16, 2018 at 15:39

Hello

Sidlauskas.David

,

Please download and update the new version

/external-link.jspa?url=http%3A%2F%2Fwww.st.com%2Fcontent%2Fst_com%2Fen%2Fproducts%2Fdevelopment-tools%2Fsoftware-development-tools%2Fstm32-software-development-tools%2Fstm32-configurators-and-code-generators%2Fstm32cubemx.html

which fix this issue.

Best Regards,

Ime,

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
Sidlauskas.David
Associate III
March 16, 2018
Posted on March 16, 2018 at 17:47

Thanks for the quick response. V 4.25.0 fixes the above issues, but there are still problems. Using the above test case and generating code for TrueStudio (Compile under root unchecked), the code will not build without errors. E.g. :

..\..\..\Src\rtc.c:73:5: warning: implicit declaration of function 'LL_PWR_EnableBkUpAccess' [-Wimplicit-function-declaration] LL_PWR_EnableBkUpAccess();

..\..\..\Src\rtc.c:75:5: warning: implicit declaration of function 'LL_APB1_GRP1_EnableClock' [-Wimplicit-function-declaration]  LL_APB1_GRP1_EnableClock(LL_APB1_GRP1_PERIPH_BKP);

..\..\..\Src\rtc.c:75:30: error: 'LL_APB1_GRP1_PERIPH_BKP' undeclared (first use in this function)

     LL_APB1_GRP1_EnableClock(LL_APB1_GRP1_PERIPH_BKP);

                            

If I generate code for the test project with the peripheral inits in main(), the project will then build without error.

Dave

ST Technical Moderator
March 22, 2018
Posted on March 22, 2018 at 15:20

Hello

Sidlauskas.David

,

I confirm this issue and it is already reported in CubeMx team for fix.

https://community.st.com/0D50X00009XkWuZSAV

Best Regards

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks