Skip to main content
martonmiklos
Senior
Jan 27, 2017 9:05 AM UTC
Solved

[CubeMX feature request]Please add an user section after the HAL_Init()

Posted on January 27, 2017 at 10:05

Dear STM32 Cube MX developers!

I am facing with the following problem, and I have not been able to find a proper solution:

I am using a STM32F103 with CDC stack via USB.

I have to add a code snippet to force the re-enumeration between the debug sessions.

Here is the generated code:

/* USER CODE BEGIN 1 */

uint8_t i, checksum;

/* USER CODE END 1 */

/* MCU Configuration----------------------------------------------------------*/

/* Reset of all peripherals, Initializes the Flash interface and the Systick. */

HAL_Init();

/* Configure the system clock */

SystemClock_Config();

/* Initialize all configured peripherals */

MX_GPIO_Init();

MX_USART1_UART_Init();

MX_USB_DEVICE_Init();

/* USER CODE BEGIN 2 */

/* USER CODE END 2 */

/* Infinite loop */

/* USER CODE BEGIN WHILE */�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?

*/

I need to add my code after the

SystemClock_Config();

but before the

MX_USB_DEVICE_Init();

I have not found any user generated sections between these two sections.

    This topic has been closed for replies.
    Sirma Siang
    Sirma SiangBest answer
    ST Employee
    Sep 12, 2017 12:08 PM UTC
    Posted on September 12, 2017 at 14:08

    USB_DEVICE user code section has been

    delivered in CubeMX4.22.1

    Kind regards

    Sirma

    15 replies

    Nesrine M_O
    Associate
    Jan 27, 2017 11:01 AM UTC
    Posted on January 27, 2017 at 12:01

    Hi

    Marton.Miklos

    ‌,

    Thanks for the suggestion! I will forward this to MX our team.

    -Nesrine-

    martonmiklos
    Senior
    Jan 27, 2017 1:16 PM UTC
    Posted on January 27, 2017 at 13:16

    Thanks for the fast response, please let me know their feedback!

    Jeanne Joly
    Associate
    Jan 30, 2017 9:59 AM UTC
    Posted on January 30, 2017 at 10:59

    Hello

    Marton.Miklos

    ,

    Just for my information and to know where we can put the user section you want, which code do you want to put between the SystemClock_config and USB_Device_Init?

    By the way, will it solve your issue if we put the user section begin and end just after the SystemClock_config (hence before the GPIO_Init)?

    BR

    Eric

    martonmiklos
    Senior
    Feb 3, 2017 9:55 AM UTC
    Posted on February 03, 2017 at 09:55

    Hello Eric,

    Thank you for your quick response!

    I am developing an USB CDC based application for a STM32F103 based board, and my board did not get re-enumerated between debug sessions unless I pull the D+ line to ground for 100 ms, (The re-enumeration would be required for the host application.)

    It is going to be an USB powered board, so this feature will not be in the final firmware, but I need it during the development.

    Technically the best would be placing user sections to all of the MX_*_Init() functions (MX_USB_DEVICE_Init in my case).

    I know the following idea would goes beyond the topic of this question, but I would recommend to extend the CubeMX code parser in such a way that users could put code everywhere between a general comment pair like this:

    /* USER CODE BEGIN Custom code */ 
    ... 
    /* USER CODE END Custom code */�?�?�?�?�?�?�?

    Jeanne Joly
    Associate
    Mar 30, 2017 10:50 AM UTC
    Posted on March 30, 2017 at 10:50

    Hello

    Marton.Miklos

    ,

    I will keep you informed as soon as we have some news about the target release where the fix will be delivered.

    BR. Eric

    Sirma Siang
    ST Employee
    Jul 6, 2017 8:53 AM UTC
    Posted on July 06, 2017 at 10:53

    Hello

    Marton.Miklos

    ,

    We propose to add a pre, and post, user code sections into MX_USB_DEVICE_Init function.

    Then it will looks like:

    void MX_USB_DEVICE_Init(void)

    {

    /* USER CODE BEGIN USB_DEVICE_Init_PreTreatment */

    /* USER CODE END USB_DEVICE_Init_PreTreatment */

    /* Init Device Library,Add Supported Class and Start the library*/

    USBD_Init(&hUsbDeviceFS, &FS_Desc, DEVICE_FS);

    USBD_RegisterClass(&hUsbDeviceFS, &USBD_AUDIO);

    USBD_AUDIO_RegisterInterface(&hUsbDeviceFS, &USBD_AUDIO_fops_FS);

    USBD_Start(&hUsbDeviceFS);

    /* USER CODE BEGIN USB_DEVICE_Init_PostTreatment */

    /* USER CODE END USB_DEVICE_Init_PostTreatment */

    }

    To be sure it will fullfill your needs, could you please share your ioc ?

    This will be in CubeMX4.23 planned in Q3 2

    Kind Regards

    Sirma

    martonmiklos
    Senior
    Jul 6, 2017 11:50 AM UTC
    Posted on July 06, 2017 at 11:50

    Hello

    ‌

    Amazing news!

    ThesePreTreatment and PosTreatment sections will be added to each function or just to the MX_USB_DEVICE_Init?

    Here is my ioc file:

    https://www.dropbox.com/s/nje8srs0gfpoqas/xlineusb.ioc?dl=0

    And here is my current code:

    /* init function */ void MX_USB_DEVICE_Init(void){ /* USER CODE BEGIN Workaround */ GPIO_InitTypeDef GPIO_InitStruct; /*Configure GPIO pin Output Level */ HAL_GPIO_WritePin(USB_R_P_GPIO_Port, USB_R_P_Pin, GPIO_PIN_RESET); /*Configure USB DP pin as GPIO */ __HAL_RCC_GPIOA_CLK_ENABLE(); GPIO_InitStruct.Pin = USB_R_P_Pin; GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW; HAL_GPIO_Init(USB_R_P_GPIO_Port, &GPIO_InitStruct); HAL_Delay(150); HAL_GPIO_WritePin(USB_R_P_GPIO_Port, USB_R_P_Pin, GPIO_PIN_SET); /* USER CODE END Workaround */ /* Init Device Library,Add Supported Class and Start the library*/ USBD_Init(&hUsbDeviceFS, &FS_Desc, DEVICE_FS); USBD_RegisterClass(&hUsbDeviceFS, &USBD_CDC); USBD_CDC_RegisterInterface(&hUsbDeviceFS, &USBD_Interface_fops_FS); USBD_Start(&hUsbDeviceFS);}�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?

    Sirma Siang
    ST Employee
    Jul 6, 2017 12:21 PM UTC
    Posted on July 06, 2017 at 12:21

    Hello

    Marton.Miklos

    ,

    As this subject is a large one, we will do it step by step, and USB_DEVICE will be the first updated.

    Thanks for your code, and ioc, sharing.

    Kind regards

    Sirma

    Sirma Siang
    Sirma SiangBest answer
    ST Employee
    Sep 12, 2017 12:08 PM UTC
    Posted on September 12, 2017 at 14:08

    USB_DEVICE user code section has been

    delivered in CubeMX4.22.1

    Kind regards

    Sirma

    martonmiklos
    Senior
    Sep 13, 2017 8:40 AM UTC
    Posted on September 13, 2017 at 08:40

    Well my usb_device.c still has the following generated contents (no user sections):

    /* init function */ void MX_USB_DEVICE_Init(void){ /* Init Device Library,Add Supported Class and Start the library*/ USBD_Init(&hUsbDeviceFS, &FS_Desc, DEVICE_FS);
     USBD_RegisterClass(&hUsbDeviceFS, &USBD_CDC);
     USBD_CDC_RegisterInterface(&hUsbDeviceFS, &USBD_Interface_fops_FS);
     USBD_Start(&hUsbDeviceFS);
    }�?�?�?�?�?�?�?�?�?

    Also the code generation fails with the following output (however this file got regenerated):

    2017-09-13 08:38:26,320 [FATAL] Middleware:652 - 
    2017-09-13 08:38:26,324 [INFO] CodeEngine:162 - oldGeneratedFile, /home/mm/STM32-workspace/xlineusb/Src/usb_device.c_save
    2017-09-13 08:38:26,420 [INFO] CodeEngine:180 - Generated code: /home/mm/STM32-workspace/xlineusb/Src/usb_device.c
    2017-09-13 08:38:26,451 [INFO] CodeEngine:162 - oldGeneratedFile, /home/mm/STM32-workspace/xlineusb/Inc/usb_device.h_save
    2017-09-13 08:38:26,516 [INFO] CodeEngine:180 - Generated code: /home/mm/STM32-workspace/xlineusb/Inc/usb_device.h
    2017-09-13 08:38:26,541 [INFO] CodeEngine:162 - oldGeneratedFile, /home/mm/STM32-workspace/xlineusb/Inc/usbd_conf.h_save
    2017-09-13 08:38:26,599 [INFO] CodeEngine:180 - Generated code: /home/mm/STM32-workspace/xlineusb/Inc/usbd_conf.h
    2017-09-13 08:38:26,621 [INFO] CodeEngine:162 - oldGeneratedFile, /home/mm/STM32-workspace/xlineusb/Src/usbd_conf.c_save
    2017-09-13 08:38:26,732 [INFO] CodeEngine:180 - Generated code: /home/mm/STM32-workspace/xlineusb/Src/usbd_conf.c
    2017-09-13 08:38:26,734 [INFO] CodeEngine:162 - oldGeneratedFile, /home/mm/STM32-workspace/xlineusb/Inc/usbd_desc.h_save
    2017-09-13 08:38:26,771 [INFO] CodeEngine:180 - Generated code: /home/mm/STM32-workspace/xlineusb/Inc/usbd_desc.h
    2017-09-13 08:38:26,773 [INFO] CodeEngine:162 - oldGeneratedFile, /home/mm/STM32-workspace/xlineusb/Src/usbd_desc.c_save
    2017-09-13 08:38:26,812 [INFO] CodeEngine:180 - Generated code: /home/mm/STM32-workspace/xlineusb/Src/usbd_desc.c
    2017-09-13 08:38:26,814 [INFO] CodeEngine:162 - oldGeneratedFile, /home/mm/STM32-workspace/xlineusb/Inc/usbd_cdc_if.h_save
    2017-09-13 08:38:26,851 [INFO] CodeEngine:180 - Generated code: /home/mm/STM32-workspace/xlineusb/Inc/usbd_cdc_if.h
    2017-09-13 08:38:26,869 [INFO] CodeEngine:162 - oldGeneratedFile, /home/mm/STM32-workspace/xlineusb/Src/usbd_cdc_if.c_save
    2017-09-13 08:38:26,916 [INFO] CodeEngine:180 - Generated code: /home/mm/STM32-workspace/xlineusb/Src/usbd_cdc_if.c
    2017-09-13 08:38:26,934 [INFO] CodeEngine:162 - oldGeneratedFile, /home/mm/STM32-workspace/xlineusb/Src/stm32f1xx_it.c_save
    2017-09-13 08:38:27,015 [INFO] CodeEngine:180 - Generated code: /home/mm/STM32-workspace/xlineusb/Src/stm32f1xx_it.c
    2017-09-13 08:38:27,041 [INFO] CodeEngine:162 - oldGeneratedFile, /home/mm/STM32-workspace/xlineusb/Inc/stm32f1xx_it.h_save
    2017-09-13 08:38:27,079 [INFO] CodeEngine:180 - Generated code: /home/mm/STM32-workspace/xlineusb/Inc/stm32f1xx_it.h
    2017-09-13 08:38:27,099 [INFO] CodeEngine:162 - oldGeneratedFile, /home/mm/STM32-workspace/xlineusb/Src/stm32f1xx_hal_msp.c_save
    2017-09-13 08:38:27,184 [INFO] CodeEngine:180 - Generated code: /home/mm/STM32-workspace/xlineusb/Src/stm32f1xx_hal_msp.c
    2017-09-13 08:38:27,187 [INFO] CodeEngine:162 - oldGeneratedFile, /home/mm/STM32-workspace/xlineusb/Src/system.tmp_save
    2017-09-13 08:38:27,225 [INFO] CodeEngine:180 - Generated code: /home/mm/STM32-workspace/xlineusb/Src/system.tmp
    2017-09-13 08:38:27,228 [INFO] CodeEngine:162 - oldGeneratedFile, /home/mm/STM32-workspace/xlineusb/Inc/stm32f1xx_hal_conf.h_save
    2017-09-13 08:38:27,275 [INFO] CodeEngine:180 - Generated code: /home/mm/STM32-workspace/xlineusb/Inc/stm32f1xx_hal_conf.h
    2017-09-13 08:38:27,287 [INFO] CodeEngine:162 - oldGeneratedFile, /home/mm/STM32-workspace/xlineusb/Inc/main.h_save
    2017-09-13 08:38:27,332 [INFO] CodeEngine:180 - Generated code: /home/mm/STM32-workspace/xlineusb/Inc/main.h
    2017-09-13 08:38:27,351 [INFO] CodeEngine:162 - oldGeneratedFile, /home/mm/STM32-workspace/xlineusb/Src/main.c_save
    2017-09-13 08:38:27,442 [INFO] CodeEngine:180 - Generated code: /home/mm/STM32-workspace/xlineusb/Src/main.c
    Exception in thread 'Thread-1222' java.lang.NoSuchMethodError: stm32Families.Families.getDefaultDefines(Ljava/lang/String;Ljava/lang/String;Ljava/lang/String;)Ljava/util/Vector;
     at com.st.microxplorer.plugins.projectmanager.engine.ProjectBuilder.searchNeededFiles(ProjectBuilder.java:1500)
     at com.st.microxplorer.plugins.projectmanager.engine.ProjectBuilder.createProject(ProjectBuilder.java:442)
     at com.st.microxplorer.plugins.projectmanager.engine.GenerateProjectThread.run(GenerateProjectThread.java:41)�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?

    Sirma Siang
    ST Employee
    Sep 13, 2017 3:43 PM UTC
    Posted on September 13, 2017 at 15:43

    Hello

    Marton.Miklos

    ,

    Have you tested with 4.1 version ?

    Mine generates the following code:

    void MX_USB_DEVICE_Init(void)

    {

    /* USER CODE BEGIN USB_DEVICE_Init_PreTreatment */

    /* USER CODE END USB_DEVICE_Init_PreTreatment */

    /* Init Device Library,Add Supported Class and Start the library*/

    USBD_Init(&hUsbDeviceFS, &FS_Desc, DEVICE_FS);

    USBD_RegisterClass(&hUsbDeviceFS, &USBD_MSC);

    USBD_MSC_RegisterStorage(&hUsbDeviceFS, &USBD_Storage_Interface_fops_FS);

    USBD_Start(&hUsbDeviceFS);

    /* USER CODE BEGIN USB_DEVICE_Init_PostTreatment */

    /* USER CODE END USB_DEVICE_Init_PostTreatment */

    }

    Or

    /* init function */

    void MX_USB_DEVICE_Init(void)

    {

    /* USER CODE BEGIN USB_DEVICE_Init_PreTreatment */

    /* USER CODE END USB_DEVICE_Init_PreTreatment */

    /* Init Device Library,Add Supported Class and Start the library*/

    USBD_Init(&hUsbDeviceFS, &FS_Desc, DEVICE_FS);

    USBD_RegisterClass(&hUsbDeviceFS, &USBD_CDC);

    USBD_CDC_RegisterInterface(&hUsbDeviceFS, &USBD_Interface_fops_FS);

    USBD_Start(&hUsbDeviceFS);

    /* USER CODE BEGIN USB_DEVICE_Init_PostTreatment */

    /* USER CODE END USB_DEVICE_Init_PostTreatment */

    }

    If you can share your ioc, I would be able to test in same conditions at my end.

    Kind regards

    Sirma