Skip to main content
valtin
Associate II
November 29, 2016
Question

CubeMX Feature Request

  • November 29, 2016
  • 1 reply
  • 617 views
Posted on November 29, 2016 at 22:26

Hello,

I like CubeMX and would like to suggest a feature for the report generator.

I use Nucleo boards a lot for development and small projects and the support for it is really great, but I always have to look up the layout of the Nucleo headers.

I usually end up on mbed.org like for the F401:

https://developer.mbed.org/platforms/ST-Nucleo-F401RE/

And I was wondering if that would not be a great thing to have in the report generated by CubeMX, alongside the pin layout already there.

I would suggest a layout similar to the mbed website with all the available ports + special functions, and also a extra column for the own pin label.

Because the basic layout is the same for the Nucleo32/64/... a general image with some custom rendered text should do the trick.

Maybe the information (like pin mapping) is also already available in CubeMX. The name/type of the Nucleo Board at least is already there.

I am looking forward hearing from you.

Sincerely Markus

#feature-request
    This topic has been closed for replies.

    1 reply

    ST Technical Moderator
    November 30, 2016
    Posted on November 30, 2016 at 08:35

    Dear User,

    Your request is reported internally to our CubeMx team.

    Thank you for fast feedback and for your contribution in the STM32 Community.

    All comments and suggestions are welcome to improve our solutions.

    Best Regards

    -Imen-

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks