Question
CubeMX 4.26 Timer with Input Capture doesn't turn off
Hi,
In CubeMX 4.25 it worked properly then I was forced to migrate my project to 4.26 and the timer with input capture stopped working properly. If I overwrite the driver with 4.25 then it works fine again. I suspect this function is wrong: HAL_TIM_IC_Stop_IT(&htim3, TIM_CHANNEL_1);
Solved: I was mistaken, it was the code optimization which was changed during migration from 4.25 to 4.26.